Hi! I'm using MSP432P401R to communicate with 25LC1024-I/SM EEPROM by SPI in polling mode. The problem is that I have to insert a delay (for loop) before reading a byte, otherwise it reads incorrectly. My code:
void Eeprom_init(void) { /* SPI Master Configuration Parameter */ const eUSCI_SPI_MasterConfig spiConfig = { // SPI mode 3 (1,1) EUSCI_A_SPI_CLOCKSOURCE_SMCLK, // SMCLK Clock Source 12000000, // SMCLK 1000000, // SPICLK EUSCI_A_SPI_MSB_FIRST, // MSB First EUSCI_A_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT, // Phase EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, // High polarity EUSCI_A_SPI_3PIN // 3Wire SPI Mode }; // Configuring pins MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P2, GPIO_PIN1 | GPIO_PIN2 | GPIO_PIN3, GPIO_PRIMARY_MODULE_FUNCTION); MAP_GPIO_setAsOutputPin(GPIO_PORT_P2, GPIO_PIN0); // !CS /* Configuring SPI in 3wire master mode */ MAP_SPI_initMaster(EUSCI_A1_BASE, &spiConfig); /* Enable SPI module */ MAP_SPI_enableModule(EUSCI_A1_BASE); /* Enabling interrupts */ //MAP_SPI_enableInterrupt(EUSCI_A1_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT); //MAP_SPI_enableInterrupt(EUSCI_A1_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT); //MAP_Interrupt_enableInterrupt(INT_EUSCIA1); Eeprom_enableCS(); Timer32_sleep_cycles(24000); // 1 ms; DCO clock 24MHz Eeprom_disableCS(); char dataRd[2]; Eeprom_readBytes(2, dataRd, 2); } void Eeprom_readBytes(uint32_t address, char data[], int length) { int i; Eeprom_enableCS(); Eeprom_spiWriteByte(E_READ); Eeprom_spiWriteByte(address >> 16); Eeprom_spiWriteByte(address >> 8); Eeprom_spiWriteByte(address); for(i = 0; i < length; i++) { data[i] = Eeprom_spiReadByte(); } Eeprom_disableCS(); } void Eeprom_spiWriteByte(uint8_t byte) { while (!(MAP_SPI_getInterruptStatus(EUSCI_A1_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT))); MAP_SPI_transmitData(EUSCI_A1_BASE, byte); while (!(MAP_SPI_getInterruptStatus(EUSCI_A1_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT))); // Dummy byte } uint8_t Eeprom_spiReadByte(void) // Adresele nescrise sunt 0xFF {
//MAP_SPI_clearInterruptFlag(EUSCI_A1_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT); while (!(MAP_SPI_getInterruptStatus(EUSCI_A1_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT))); MAP_SPI_transmitData(EUSCI_A1_BASE, 0xFF); int jj; for(jj=0;jj<50;jj++); //while (!(MAP_SPI_getInterruptStatus(EUSCI_A1_BASE, EUSCI_A_SPI_RECEIVE_INTERRUPT))); return MAP_SPI_receiveData(EUSCI_A1_BASE); }
With the for loop in Eeprom_spiReadByte() it reads 0x11FF which is the expected value. This is the logic analyzer capture.
Without the loop, it reads 0x0011 which should be 0x11FF.
Any ideas what I am doing wrong? Why is the delay necessary and why doesn't the code work by just polling the receive interrupt in Eeprom_spiReadByte()?