This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What is the recommended way to measure sensor with higher voltage than the
Differential input voltage range with internal reference?
As per the datasheet SD24's input range is ±928mV (@SD24GAINx = 1) but our
sensor output is 0 to 1.6V, so this cannot be directly fed into the SD24 input
and it may be necessary to add a circuit to float the minus side, so that may require an external reference IC.
Please let me know your suggestions and if there is any application notes
or guide on using MSP430's SD24.Should we choose external ADC in this case?
Best Regards
paddu
The Sigma Delta ADC is targeted towards differential inputs. If you want to use it with a single-ended input configuration, you're going to limit the ADC performance as you mentioned. I would recommend a SAR ADC for single-ended inputs although I know the Sigma Delta ADC's have higher resolution but may have worse dynamic range performance.
SD16 single-ended noise problem - MSP low-power microcontroller forum - MSP low-power microcontrollers...
Regards,
James
MSP Customer Applications
**Attention** This is a public forum