Part Number: MSP430I2041
Other Parts Discussed in Thread: EVM430-I2040S,
Hi,
What is the recommended way to measure sensor with higher voltage than the
Differential input voltage range with internal reference?
As per the datasheet SD24's input range is ±928mV (@SD24GAINx = 1) but our
sensor output is 0 to 1.6V, so this cannot be directly fed into the SD24 input
and it may be necessary to add a circuit to float the minus side, so that may require an external reference IC.
Please let me know your suggestions and if there is any application notes
or guide on using MSP430's SD24.Should we choose external ADC in this case?
Best Regards
paddu