Part Number: MSP430F233
Tool/software: Code Composer Studio
I have two boards (both with MSP430F233 chips) that I am trying to communicate with over UART. I have flashed one of my boards to transmit a continuous stream of data (32-bits long), and my second board is receiving the data. Both UARTS are configured at a baud rate of 115200, and my DCO is set 8 MHz with SMCLK enabled. I have tried reading the contents of the RX Buffer and every time I read the buffer I notice that the UCOE, UCFE, and UCRXERR error flag is raised within my debug session. I know that this means that the data isn't being read in quick enough, which is causing for my last couple bytes of data to be overwritten and corrupted. I am sort of new to programming these particular MCUs are there any good solutions which could fix this error and clear the UCOE error when read?
Thanks!