Part Number: MSP430I2020
Hello,
regarding the PGA customer would like to know how the gain error (Eg) differs between the different PGA settings.
In the data sheet the Eg parameter is specified for SD24GAINx=1,8,16 with Min -1% and Max +1%. What does this exactly mean ?
- Can each channel deviate -1 to +1% from the gain spec ?
- Can a gain of 1 have a -1% gain error while a gain 8 will have a +0.5% gain error ?
- Or will all gains have the same gain error of -0.5% ? Or even the same absolute error.
- What is the case with the gains 2 and 4 as they are not listed ?
Customer has dynamically switching between multiple gain settings, and are planning to calibrate only one gain.
Regards, Holger