Other Parts Discussed in Thread: CC430F5137
Hello All,
I am currently working on CC430F5137 BSL for Firmware Update feature.
I am able to
- enter into BSL mode
- Mass Erase Flash
- Rx Password and Unlock otehr commands
But i can not write a new data Block into the Flash.
While giving RX Data Block Command with any dummy data and dummy address like:
$80 $08 $00 $10 $00 $3c $00 $31 $40 $00 $5c $6c $f4
I am getting following Response:
00 80 02 00 3B 01 41 D4
Checking out Error code in Documentation, It says:
0x01 : Flash Write Check Failed. After programming, a CRC is run on the programmed data. If the CRC does not match the expected result, this error is returned.
Please let me know if anyone has found similar problem and has a solution for it.
Thank you.