Part Number: MSP430F5529
Other Parts Discussed in Thread: MSP430WARE
Tool/software: Code Composer Studio
I am trying to interface the o-led with the Micro controller , But i am having trouble with interrupt part of the code , the interrupt routine does not get triggered after buffer is loaded with 0x80 during initialization oled.
The code is
//******************************************************************************
// MSP430F552x Demo - USCI_B0, I2C Master multiple byte TX/RX
//
// Description: I2C master communicates to I2C slave sending and receiving
// 3 different messages of different length. I2C master will enter LPM0 mode
// while waiting for the messages to be sent/receiving using I2C interrupt.
// ACLK = NA, MCLK = SMCLK = DCO 16MHz.
//
// /|\ /|\
// MSP430F5529 4.7k |
// ----------------- | 4.7k
// /|\ | P3.1|---+---|-- I2C Clock (UCB0SCL)
// | | | |
// ---|RST P3.0|-------+-- I2C Data (UCB0SDA)
// | |
// | |
// | |
// | |
// | |
// | |
//
// Nima Eskandari
// Texas Instruments Inc.
// April 2017
// Built with CCS V7.0
//******************************************************************************
#include <msp430.h>
#include <stdint.h>
#include <stdbool.h>
//******************************************************************************
// Example Commands ************************************************************
//******************************************************************************
#define TYPE_0_LENGTH 1
#define TYPE_1_LENGTH 2
#define command_write 0x80
uint8_t SSD1306_LCDWIDTH[TYPE_0_LENGTH]={128};
uint8_t SSD1306_LCDHEIGHT[TYPE_0_LENGTH]= {64};
uint8_t SSD1306_SETCONTRAST[TYPE_1_LENGTH]={0x81,0xCF};
uint8_t SSD1306_DISPLAYALLON_RESUME[TYPE_0_LENGTH]={0xA4};
uint8_t SSD1306_DISPLAYALLON[TYPE_0_LENGTH]={0xA5};
uint8_t SSD1306_NORMALDISPLAY[TYPE_0_LENGTH]={0xA6};
uint8_t SSD1306_INVERTDISPLAY[TYPE_0_LENGTH]={0xA7};
uint8_t SSD1306_DISPLAYOFF[TYPE_0_LENGTH]={0xAE};
uint8_t SSD1306_DISPLAYON[TYPE_0_LENGTH]={0xAF};
uint8_t SSD1306_SETDISPLAYOFFSET[TYPE_1_LENGTH]={0xD3,0x00};
uint8_t SSD1306_SETCOMPINS[TYPE_1_LENGTH]={0xDA,0x02};
uint8_t SSD1306_SETVCOMDETECT[TYPE_1_LENGTH]={0xDB,0x40};
uint8_t SSD1306_SETDISPLAYCLOCKDIV[TYPE_1_LENGTH]={0xD5,0x80};
uint8_t SSD1306_SETPRECHARGE[TYPE_1_LENGTH]={0xD9,0xF1};
uint8_t SSD1306_SETMULTIPLEX[TYPE_1_LENGTH]={0xA8,0x35};
uint8_t SSD1306_SETLOWCOLUMN[TYPE_0_LENGTH]={0x00};
uint8_t SSD1306_SETHIGHCOLUMN[TYPE_0_LENGTH]={0x10};
uint8_t SSD1306_SETSTARTLINE[TYPE_0_LENGTH]={0x40};
uint8_t SSD1306_MEMORYMODE[TYPE_1_LENGTH]={0x20,0x00};
uint8_t SSD1306_COLUMNADDR[TYPE_0_LENGTH]={0x21};
uint8_t SSD1306_PAGEADDR[TYPE_0_LENGTH]={0x22};
uint8_t SSD1306_COMSCANINC[TYPE_0_LENGTH]={0xC0};
uint8_t SSD1306_COMSCANDEC[TYPE_0_LENGTH]={0xC8};
uint8_t SSD1306_SEGREMAP[TYPE_0_LENGTH]={0xA0|0x1};
uint8_t SSD1306_CHARGEPUMP[TYPE_1_LENGTH]={0x8D,0x14};
uint8_t SSD1306_EXTERNALVCC[TYPE_0_LENGTH]={0x1};
uint8_t SSD1306_SWITCHCAPVCC[TYPE_0_LENGTH]={0x2};
//uint8_t CLOCKDIVRATIO[TYPE_0_LENGTH]={0x80};
uint8_t MULTIPLEX_RATIO[TYPE_0_LENGTH]={0x3F};
uint8_t SETTING_DISPLAY_ON_OFF[TYPE_0_LENGTH]={0x00};
uint8_t CHARGEPUMPCONFIG[TYPE_0_LENGTH]={0x14};
uint8_t CONFIGURINGCOMPIN[TYPE_0_LENGTH]={0x12};
uint8_t SETTINGTOHORIZONTALMODE[TYPE_0_LENGTH]={0x00};
uint8_t CONTRASTVALUE[TYPE_0_LENGTH]={0xCF};
uint8_t PRECHARGEPERIOD[TYPE_0_LENGTH]={0xF1};
uint8_t VCOM_DESELECT_LEVEL[TYPE_0_LENGTH]={0X40};
#define Slaveadress 0x78
/* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
* The slave will send example SlaveTypeX buffers in response.
*
* CMD_TYPE_X_MASTER are example commands the master sends to the slave.
* The slave will initialize itself to receive MasterTypeX example buffers.
* */
#define CMD_TYPE_0_SLAVE 0
#define CMD_TYPE_1_SLAVE 1
#define CMD_TYPE_2_SLAVE 2
#define CMD_TYPE_0_MASTER 3
#define CMD_TYPE_1_MASTER 4
#define CMD_TYPE_2_MASTER 5
#define TYPE_0_LENGTH 1
#define TYPE_1_LENGTH 2
#define TYPE_2_LENGTH 6
#define MAX_BUFFER_SIZE 20
#define mastertype 0x00
/* MasterTypeX are example buffers initialized in the master, they will be
* sent by the master to the slave.
* SlaveTypeX are example buffers initialized in the slave, they will be
* sent by the slave to the master.
* */
//uint8_t MasterType2 [TYPE_2_LENGTH] = {'F', '4', '1', '9', '2', 'B'};
//uint8_t MasterType1 [TYPE_1_LENGTH] = { 8, 9};
//uint8_t MasterType0 [TYPE_0_LENGTH] = { 11};
//
//
//uint8_t SlaveType2 [TYPE_2_LENGTH] = {0};
//uint8_t SlaveType1 [TYPE_1_LENGTH] = {0};
//uint8_t SlaveType0 [TYPE_0_LENGTH] = {0};
//******************************************************************************
// General I2C State Machine ***************************************************
//******************************************************************************
typedef enum I2C_ModeEnum{
IDLE_MODE,
NACK_MODE,
TX_REG_ADDRESS_MODE,
RX_REG_ADDRESS_MODE,
TX_DATA_MODE,
RX_DATA_MODE,
SWITCH_TO_RX_MODE,
SWITHC_TO_TX_MODE,
TIMEOUT_MODE
} I2C_Mode;
/* Used to track the state of the software state machine*/
I2C_Mode MasterMode = IDLE_MODE;
/* The Register Address/Command to use*/
uint8_t TransmitRegAddr = 0;
/* ReceiveBuffer: Buffer used to receive data in the ISR
* RXByteCtr: Number of bytes left to receive
* ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
* TransmitBuffer: Buffer used to transmit data in the ISR
* TXByteCtr: Number of bytes left to transfer
* TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
* */
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t RXByteCtr = 0;
uint8_t ReceiveIndex = 0;
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t TXByteCtr = 0;
uint8_t TransmitIndex = 0;
/* I2C Write and Read Functions */
/* For slave device with dev_addr, writes the data specified in *reg_data
*
* dev_addr: The slave device address.
* Example: SLAVE_ADDR
* reg_addr: The register or command to send to the slave.
* Example: CMD_TYPE_0_MASTER
* *reg_data: The buffer to write
* Example: MasterType0
* count: The length of *reg_data
* Example: TYPE_0_LENGTH
* */
I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count);
/* For slave device with dev_addr, read the data specified in slaves reg_addr.
* The received data is available in ReceiveBuffer
*
* dev_addr: The slave device address.
* Example: SLAVE_ADDR
* reg_addr: The register or command to send to the slave.
* Example: CMD_TYPE_0_SLAVE
* count: The length of data to read
* Example: TYPE_0_LENGTH
* */
I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count);
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);
I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count)
{
/* Initialize state machine */
MasterMode = TX_REG_ADDRESS_MODE;
TransmitRegAddr = reg_addr;
RXByteCtr = count;
TXByteCtr = 0;
ReceiveIndex = 0;
TransmitIndex = 0;
/* Initialize slave address and interrupts */
UCB0I2CSA = dev_addr;
UCB0IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts
UCB0IE &= ~UCRXIE; // Disable RX interrupt
UCB0IE |= UCTXIE; // Enable TX interrupt
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts
return MasterMode;
}
I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
/* Initialize state machine */
MasterMode = TX_REG_ADDRESS_MODE;
TransmitRegAddr = reg_addr;
//Copy register data to TransmitBuffer
CopyArray(reg_data, TransmitBuffer, count);
TXByteCtr = count;
RXByteCtr = 0;
ReceiveIndex = 0;
TransmitIndex = 0;
/* Initialize slave address and interrupts */
UCB0I2CSA = dev_addr;
UCB0IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts
UCB0IE &= ~UCRXIE; // Disable RX interrupt
UCB0IE |= UCTXIE; // Enable TX interrupt
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
// __bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts
//__delay_cycles(2000000);
return MasterMode;
}
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
uint8_t copyIndex = 0;
for (copyIndex = 0; copyIndex < count; copyIndex++)
{
dest[copyIndex] = source[copyIndex];
}
}
//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************
void initClockTo16MHz()
{
UCSCTL3 |= SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5; // Select DCO range 16MHz operation
UCSCTL2 = FLLD_0 + 487; // Set DCO Multiplier for 16MHz
// (N + 1) * FLLRef = Fdco
// (487 + 1) * 32768 = 16MHz
// Set FLL Div = fDCOCLK
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 16 MHz / 32,768 Hz = 500000 = MCLK cycles for DCO to settle
__delay_cycles(500000);//
// Loop until XT1,XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG); // Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
}
uint16_t setVCoreUp(uint8_t level){
uint32_t PMMRIE_backup, SVSMHCTL_backup, SVSMLCTL_backup;
//The code flow for increasing the Vcore has been altered to work around
//the erratum FLASH37.
//Please refer to the Errata sheet to know if a specific device is affected
//DO NOT ALTER THIS FUNCTION
//Open PMM registers for write access
PMMCTL0_H = 0xA5;
//Disable dedicated Interrupts
//Backup all registers
PMMRIE_backup = PMMRIE;
PMMRIE &= ~(SVMHVLRPE | SVSHPE | SVMLVLRPE |
SVSLPE | SVMHVLRIE | SVMHIE |
SVSMHDLYIE | SVMLVLRIE | SVMLIE |
SVSMLDLYIE
);
SVSMHCTL_backup = SVSMHCTL;
SVSMLCTL_backup = SVSMLCTL;
//Clear flags
PMMIFG = 0;
//Set SVM highside to new level and check if a VCore increase is possible
SVSMHCTL = SVMHE | SVSHE | (SVSMHRRL0 * level);
//Wait until SVM highside is settled
while((PMMIFG & SVSMHDLYIFG) == 0)
{
;
}
//Clear flag
PMMIFG &= ~SVSMHDLYIFG;
//Check if a VCore increase is possible
if((PMMIFG & SVMHIFG) == SVMHIFG)
{
//-> Vcc is too low for a Vcore increase
//recover the previous settings
PMMIFG &= ~SVSMHDLYIFG;
SVSMHCTL = SVSMHCTL_backup;
//Wait until SVM highside is settled
while((PMMIFG & SVSMHDLYIFG) == 0)
{
;
}
//Clear all Flags
PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
SVMLVLRIFG | SVMLIFG |
SVSMLDLYIFG
);
//Restore PMM interrupt enable register
PMMRIE = PMMRIE_backup;
//Lock PMM registers for write access
PMMCTL0_H = 0x00;
//return: voltage not set
return false;
}
//Set also SVS highside to new level
//Vcc is high enough for a Vcore increase
SVSMHCTL |= (SVSHRVL0 * level);
//Wait until SVM highside is settled
while((PMMIFG & SVSMHDLYIFG) == 0)
{
;
}
//Clear flag
PMMIFG &= ~SVSMHDLYIFG;
//Set VCore to new level
PMMCTL0_L = PMMCOREV0 * level;
//Set SVM, SVS low side to new level
SVSMLCTL = SVMLE | (SVSMLRRL0 * level) |
SVSLE | (SVSLRVL0 * level);
//Wait until SVM, SVS low side is settled
while((PMMIFG & SVSMLDLYIFG) == 0)
{
;
}
//Clear flag
PMMIFG &= ~SVSMLDLYIFG;
//SVS, SVM core and high side are now set to protect for the new core level
//Restore Low side settings
//Clear all other bits _except_ level settings
SVSMLCTL &= (SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 +
SVSMLRRL1 + SVSMLRRL2
);
//Clear level settings in the backup register,keep all other bits
SVSMLCTL_backup &=
~(SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 + SVSMLRRL1 + SVSMLRRL2);
//Restore low-side SVS monitor settings
SVSMLCTL |= SVSMLCTL_backup;
//Restore High side settings
//Clear all other bits except level settings
SVSMHCTL &= (SVSHRVL0 + SVSHRVL1 +
SVSMHRRL0 + SVSMHRRL1 +
SVSMHRRL2
);
//Clear level settings in the backup register,keep all other bits
SVSMHCTL_backup &=
~(SVSHRVL0 + SVSHRVL1 + SVSMHRRL0 + SVSMHRRL1 + SVSMHRRL2);
//Restore backup
SVSMHCTL |= SVSMHCTL_backup;
//Wait until high side, low side settled
while(((PMMIFG & SVSMLDLYIFG) == 0) &&
((PMMIFG & SVSMHDLYIFG) == 0))
{
;
}
//Clear all Flags
PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
SVMLVLRIFG | SVMLIFG | SVSMLDLYIFG
);
//Restore PMM interrupt enable register
PMMRIE = PMMRIE_backup;
//Lock PMM registers for write access
PMMCTL0_H =0x00;
return true;
}
bool increaseVCoreToLevel2()
{
uint8_t level = 2;
uint8_t actlevel;
bool status = true;
//Set Mask for Max. level
level &= PMMCOREV_3;
//Get actual VCore
actlevel = PMMCTL0 & PMMCOREV_3;
//step by step increase or decrease
while((level != actlevel) && (status == true))
{
if(level > actlevel)
{
status = setVCoreUp(++actlevel);
}
}
return (status);
}
void initGPIO()
{
//LEDs
P1OUT =0x00; // P1 setup for LED & reset output
P1DIR |= BIT0;
P4DIR |= BIT7;
P4OUT &= ~(BIT7);
//I2C Pins
P3SEL |= BIT0 + BIT1; // P3.0,1 option select
}
void initI2C()
{
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = 255; // fSCL = SMCLK/160 = ~100kHz
UCB0BR1 = 0;
UCB0I2CSA = Slaveadress; // Slave Address is 048h
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
UCB0IE |= UCNACKIE;
}
void delay(int x)
{
int i,j,k;
for(i=0;i<32000;i++)
{
for(k=0;k<32000;k++)
for(j=0;j<32000;j++)
for(;x>0;x--);
}
}
void writecommand(uint8_t cmd)
{
uint8_t cmd_array[TYPE_0_LENGTH]={cmd};
I2C_Master_WriteReg(Slaveadress,command_write,cmd_array,TYPE_0_LENGTH);
}
void writedata(uint8_t dat)
{
uint8_t data_array[TYPE_0_LENGTH]={dat};
I2C_Master_WriteReg(Slaveadress,0x40,data_array,TYPE_0_LENGTH);
}
void oled_start()
{
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_DISPLAYOFF, TYPE_0_LENGTH);
delay(32000);
// I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_NORMALDISPLAY,TYPE_0_LENGTH);
//I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETDISPLAYCLOCKDIV, TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETMULTIPLEX,TYPE_1_LENGTH);
delay(32000);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETDISPLAYOFFSET,TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETSTARTLINE,TYPE_0_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SEGREMAP,TYPE_0_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_COMSCANDEC,TYPE_0_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETCOMPINS,TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETCONTRAST,TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_DISPLAYALLON_RESUME,TYPE_0_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_NORMALDISPLAY,TYPE_0_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETDISPLAYCLOCKDIV, TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_CHARGEPUMP,TYPE_1_LENGTH) ;
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_MEMORYMODE,TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETPRECHARGE,TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_SETVCOMDETECT,TYPE_1_LENGTH);
I2C_Master_WriteReg(Slaveadress,command_write,SSD1306_DISPLAYON,TYPE_0_LENGTH);
}
//******************************************************************************
// Main ************************************************************************
// Send and receive three messages containing the example commands *************
//******************************************************************************
//void set_contrast(void)
//{
// I2C_Master_WriteReg(Slaveadress,0x40,55,TYPE_0_LENGTH);
//}
void init_write(void)
{
writecommand(0x00);
writecommand(0x21);
writecommand(0x00);
writecommand(0x7F);
writecommand(0x22);
writecommand(0x00);
writecommand(0x07);
}
void setXY(uint8_t row,uint8_t col)
{
writecommand(0xb0+row); //set page address
writecommand(0x00+(8*col&0x0f)); //set low col address
writecommand(0x10+((8*col>>4)&0x0f)); //set high col address
}
int main(void) {
WDTCTL = WDTPW | WDTHOLD;
// Stop watchdog timer
//int Sadress=0x78;
// int contra[TYPE_0_LENGTH]={255};
increaseVCoreToLevel2();
initClockTo16MHz();
initGPIO();
__enable_interrupt();
initI2C();
oled_start();
init_write();
// writecommand(0x2E); // END SCROLLING
// set_contrast();
// I2C_Master_WriteReg(Sadress, CMD_TYPE_0_MASTER, MasterType0, TYPE_0_LENGTH);
// I2C_Master_WriteReg(Sadress, CMD_TYPE_1_MASTER, MasterType1, TYPE_1_LENGTH);
// I2C_Master_WriteReg(Sadress, CMD_TYPE_2_MASTER, MasterType2, TYPE_2_LENGTH);
// I2C_Master_ReadReg(SLAVE_ADDR, CMD_TYPE_0_SLAVE, TYPE_0_LENGTH);
// CopyArray(ReceiveBuffer, SlaveType0, TYPE_0_LENGTH);
// I2C_Master_ReadReg(SLAVE_ADDR, CMD_TYPE_1_SLAVE, TYPE_1_LENGTH);
//CopyArray(ReceiveBuffer, SlaveType1, TYPE_1_LENGTH);
// I2C_Master_ReadReg(SLAVE_ADDR, CMD_TYPE_2_SLAVE, TYPE_2_LENGTH);
//CopyArray(ReceiveBuffer, SlaveType2, TYPE_2_LENGTH);
__bis_SR_register(LPM0_bits + GIE);
return 0;
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_B0_VECTOR
__interrupt void USCI_B0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCI_B0_ISR (void)
#else
#error Compiler not supported!
#endif
{
//Must read from UCB0RXBUF
uint8_t rx_val = 0;
switch(__even_in_range(UCB0IV,0xC0))
{
case USCI_NONE:break; // Vector 0 - no interrupt
case USCI_I2C_UCALIFG:break; // Interrupt Vector: I2C Mode: UCALIFG
case USCI_I2C_UCNACKIFG:break; // Interrupt Vector: I2C Mode: UCNACKIFG
case USCI_I2C_UCSTTIFG:break; // Interrupt Vector: I2C Mode: UCSTTIFG
case USCI_I2C_UCSTPIFG:break; // Interrupt Vector: I2C Mode: UCSTPIFG
case USCI_I2C_UCRXIFG:
rx_val = UCB0RXBUF;
if (RXByteCtr)
{
ReceiveBuffer[ReceiveIndex++] = rx_val;
RXByteCtr--;
}
if (RXByteCtr == 1)
{
UCB0CTL1 |= UCTXSTP;
}
else if (RXByteCtr == 0)
{
UCB0IE &= ~UCRXIE;
MasterMode = IDLE_MODE;
__bic_SR_register_on_exit(CPUOFF); // Exit LPM0
}
break; // Interrupt Vector: I2C Mode: UCRXIFG
case USCI_I2C_UCTXIFG:
switch (MasterMode)
{
case TX_REG_ADDRESS_MODE:
UCB0TXBUF = TransmitRegAddr;
//__delay_cycles(6000000);
delay(32000);
if (RXByteCtr)
MasterMode = SWITCH_TO_RX_MODE; // Need to start receiving now
else
MasterMode = TX_DATA_MODE; // Continue to transmission with the data in Transmit Buffer
break;
case SWITCH_TO_RX_MODE:
UCB0IE |= UCRXIE; // Enable RX interrupt
UCB0IE &= ~UCTXIE; // Disable TX interrupt
UCB0CTL1 &= ~UCTR; // Switch to receiver
MasterMode = RX_DATA_MODE; // State state is to receive data
UCB0CTL1 |= UCTXSTT; // Send repeated start
if (RXByteCtr == 1)
{
//Must send stop since this is the N-1 byte
while((UCB0CTL1 & UCTXSTT));
UCB0CTL1 |= UCTXSTP; // Send stop condition
}
break;
case TX_DATA_MODE:
if (TXByteCtr)
{
UCB0TXBUF = TransmitBuffer[TransmitIndex++];
TXByteCtr--;
}
else
{
//Done with transmission
UCB0CTL1 |= UCTXSTP; // Send stop condition
MasterMode = IDLE_MODE;
UCB0IE &= ~UCTXIE; // disable TX interrupt
//__bic_SR_register_on_exit(CPUOFF); // Exit LPM0
}
break;
default:
__no_operation();
break;
}
break; // Interrupt Vector: I2C Mode: UCTXIFG
default: break;
}
}