Hello,
I'm a university student. I have being using PIC microcontrollers. I want to learn and use MSP430 microcontrollers from now on. I browsed the official TI page for a programmer solution to see that there was only two of them, and the cheapest one is 200$! USB interfaced one is 340$. Actually, I don't have that much money, or I can say, I don't want to (can't) pay that much money for a programmer.
Instead, I'm looking for a cheaper third party programmer with these features:
1) Must program all the MSP430 product families
2) I won't use a development board, I will run it on a simple bread-board (like I have always done with PIC microcontrollers). Either ISCP port or ZIF socket will be sufficient.
3) I prefer one with USB with PC
4) It can be slow but should be as cheap as possible
Actually, I have already found a programmer:
http://www.olimex.com/dev/msp-jtag-tiny.html
But I wanted to consult you experienced people before purchasing anything.
Any help will be appreciated.