Other Parts Discussed in Thread: SYSBIOS, MSP430F5257
Tool/software: TI-RTOS
HI
Today, I'm try to porting 5529 projects to 5259, modified cmd and ccxml files, and Predefined Symbols (__MSP430F5259__) , then the following error occurs when I rebuild the projects.
Description Resource Path Location Type
gmake: *** No rule to make target 'build-601269185', needed by 'configPkg/compiler.opt'. CMS_MSP430F5259_TIRTOS C/C++ Problem
gmake: Target 'all' not remade because of errors. CMS_MSP430F5259_TIRTOS C/C++ Problem
gmake[1]: *** [build-601269185-inproc] Error 1 CMS_MSP430F5259_TIRTOS C/C++ Problem
xdc.cfg.Program : The package 'ti.sysbios.family.msp430' is not compatible with XDCtools used in this build. Please either use XDCtools compatible with that package, or update the product containing that package, or rebuild the package with XDCtools 3.50 or later. .xdchelp /CMS_MSP430F5259_TIRTOS line 71 C/C++ Problem
NOTE: This is not the previous mistake. The previous error was "......... ti/drivers/lib/drivers_MSP430F52599.ae430X can't find" so I recompile sysbois and ti-driver based on
The goal is to produce the following files
drivers_MSP430F5257.ae430X
drivers_MSP430F5257.ae430X.mak
drivers_MSP430F5257_instrumented.ae430X
drivers_MSP430F5257_instrumented.ae430X.mak
But I had the following problems during the compilation process
Error: The compiler in f:/Program is not compatible with this version of TI-RTOS or SYS/BIOS. Please use Arm compiler 5.2.2 or newer.
But my ccs7.4 compiler is already TI v16.9.6.LTS , I don't know how to change it.
and ti-cgt-arm_16.9.6.LTS should be the latest version of the arm compiler
version: bios_6_46_00_23 msp430_driverlib_2_70_01_01a xdc_toools_3_32_00_00_06
Somebody help me? thank you.
best regrads
xc.mo