Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
i have a problem with MSP432 and BSL Invoke.
If i the Hardware BSL Invoke funktion call is right at begin of the program code everything works like this:
int main(void)
{
volatile uint32_t ii;
/* Halting the Watchdog */
MAP_WDT_A_holdTimer();
//Old Board with PUMP PWM on P6.6 and P6.7
MSP432_Clock_init();
// GPIO_setAsOutputPin(GPIO_PORT_P3, GPIO_PIN0);
// GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
if(CheckFlashMailbox(COMMAND_BSL_CONFIG) !=BOOT_OVERRIDE_AND_MAILBOX_OPERATIONS_SUCCESS)
{
// GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
if((P1->IN & BIT0)==1)
{
// SysCtl_rebootDevice();
BSL_INVOKE(BSL_CONFIG_HW_INVOKE_PORT1 | BSL_CONFIG_HW_INVOKE_PIN0 |
BSL_CONFIG_HW_INVOKE | BSL_CONFIG_HW_INVOKE_PIN_HIGH |
BSL_CONFIG_INTERFACE_UART);
}
}
If i call this function right after some initialisation it doesnt responde to BSL Scripter at all.
Why is it like this?
If i software BSL invoke like sending a UART command and i call then this function:
BSL_INVOKE(BSL_CONFIG_HW_INVOKE_PORT1 | BSL_CONFIG_HW_INVOKE_PIN0 | BSL_CONFIG_HW_INVOKE | BSL_CONFIG_HW_INVOKE_PIN_HIGH | BSL_CONFIG_INTERFACE_UART);
It also doenst work.
Can anyone help me?
OBs: I am flashing the MSP432 througth BSL Scripter.