This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/EZ430-RF2500-SEH: Writing source code to AP/ED in CCS/CCE

Part Number: EZ430-RF2500-SEH


Tool/software: Code Composer Studio

Hello, I purchased the dev kit ez430-rf2500-seh and having ensured that the Sensor Monitor application works correct, I tried to write my own code to the access point. I did it - it now flashes the LED, but I would like to go back to the demo code which was there before I overwrote it with my own code. Unfortunately, I cannot do it in my CCS v4 (included on the CD). I have the following error while trying to build the imported project: C:\Program Files (x86)\Texas Instruments\ccsv4\utils\gmake\gmake: *** No rule to make target `Peer Applications/SEH_ED_v1.5.obj'.  Stop.

I don't know what to do, as all required files should be there - I didn't change anything, just installed everything from the CD. Also, my project branch works like this (see photo), it has some weird exclamation marks.

I would appreciate if anyone could help me with this, as I cannot even go back to the very beginning. Maybe any of You have correct files to import the demo project correctly.

**Attention** This is a public forum