Part Number: MSP432P401R
I'm spinning a board where I'm essentially using a FT232R chip for a back channel uart interface and for powering my board. In the FT232R manual it mentions various concerns with how much current my application will draw. For example, below (see attachment) or page 23 of FT232R datasheet under section "USB Bus Powered Configuration (http://www.ftdichip.com/Support/Documents/DataSheets/ICs/DS_FT232R.pdf) is the page describing some of these "Basic rules" as they call them. My questions specifically are...
1) How much current will a MSP432 draw (is it greater than 100mA)?
2) When sourcing power to the MSP432 can I come right off the Vcc connection shown below (also should it be before or after the Ferrite Bead)?
3) Should I use any additional caps on the Vcc line coming into the Vcc pins of the MSP432?