This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2274: Using PxSEL register to select between different peripherals?

Part Number: MSP430F2274

In the MSP430F2274 there is no P1SEL2 register, only P1SEL and P2SEL. When looking at the datasheet, there are three different options to select from using the P1SEL register. If there is no P1SEL2 register how could I select the third option of the peripherals?

For instance, pin P1.0 has the options of GPIO, Timer_A clock signal TACLK input, and ADC10 conversion clock. If there is no P1SEL2 register, how can the third option be selected?

**Attention** This is a public forum