Other Parts Discussed in Thread: MSP-FET,
Hi,
I have a small production with the MSP430G2452IPW20R and have problems with the programming process. The programming interface uses pin 17 (TEST) and pin 16 (/RST) with a 47k pull up resistance. All wires are kept short. I'm using the MSP-FET programmer and the MSPFlasher 1.3.8 within a batch process. Sometimes, the uC is not working after programming. Unfortunately does the fuse bit is set and therefore I need to replace the uC (SMD!).
Under development I also noted some instability. Sometimes I was not able to reprogram the uC with the MSP-FET. So I needed to program it using the LaunchPad and than it was possible to use the MSP-FET again (all without setting the fuse bit)
Does someone has an explanation and workaround?
Kind regards