Hi,
Brief: Serial eUSCI_A0 does not transmit any serial data to host PC.
I have started developing with the EVM and tried to configure and use serial UART on eUSCI_A0. On the EVM it should communicate thru the ezFET once the pins on header J2 are populated (shown below):
I have configured eUSCI_A0 register as shown:
void serial_init(void)
{
EUSCI_A_UART_initParam param = {0};
param.selectClockSource = EUSCI_A_UART_CLOCKSOURCE_SMCLK; //SMCLK=> (DCO)16MHz/DIVS_4 -------- ACLK=LFXTCLK=37.768 Khz
param.clockPrescalar = 69; //57600 on 4 MHZ
param.firstModReg = 0;
param.secondModReg = 4;
param.parity = EUSCI_A_UART_NO_PARITY;
param.msborLsbFirst = EUSCI_A_UART_LSB_FIRST;
param.numberofStopBits = EUSCI_A_UART_ONE_STOP_BIT;
param.uartMode = EUSCI_A_UART_MODE;
param.overSampling = EUSCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;
// Sets P2SEL1.x
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P2, GPIO_PIN0 + GPIO_PIN1, GPIO_SECONDARY_MODULE_FUNCTION);// P2.0 UCA0TXD and P2.1 UCA0RXD
if (STATUS_FAIL == EUSCI_A_UART_init(EUSCI_A0_BASE, ¶m)) {
return;
}
PMM_unlockLPM5();
EUSCI_A_UART_enable(EUSCI_A0_BASE);
EUSCI_A_UART_clearInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT);
EUSCI_A_UART_clearInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_TRANSMIT_INTERRUPT);
EUSCI_A_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_TRANSMIT_INTERRUPT); // Enable interrupt
// Enable USCI_A0 RX interrupt
EUSCI_A_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT); // Enable interrupt
__enable_interrupt();
}
Here is the clock init routine:
void clock_init(void)
{
/*
* Configure CS module
* MCLK = 16 MHz from DCOCLK
* SMCLK = 8MHz from DCOCLK
* ACLK = LFXTCLK 32.768 KHz
*/
// Unlock CS registers
CSCTL0_H = CSKEY >> 8;
// Set DCO to 16MHz
CSCTL1 = DCORSEL | DCOFSEL_4;
// SELA selects ACLK source
// SELS selects SMCLK source
// SELM selects MCLK source
// For EVM HFXCLK = 8MHz, LFXCLK = 32.768 kHz,
// Set ACLK = LFXTCLK, SMCLK = DCO, MCLK = HFXTCLK
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__HFXTCLK;
// DIVA selects ACLK source divider
// DIVS selects SMCLK source divider
// DIVM selects MCLK source divider
CSCTL3 = (DIVA__1 | DIVS__4 | DIVM__1);
CSCTL4 &= (HFXTDRIVE_0);
CSCTL4 &= (HFXTBYPASS_0);
CSCTL4 |= (HFFREQ_1);
CSCTL4 |= (LFXTDRIVE_3);
CSCTL4 |= (LFXTBYPASS_0);
CSCTL4 &= ~(HFXTOFF);
CSCTL4 &= ~(LFXTOFF);
// Lock CS register
CSCTL0_H = 0; //
}
On debug the UCA0 Registers are shown below:
MAIN:
uint8_t RXData = 0, TXData = 0;
uint8_t check = 0;
int main(void) {
uint32_t i = 0;
TXData = 0x01;
while(1){
serial_trasmitDataByte(TXData);
// TXData = TXData+1;
for(i = 0; i < 100000; i++);
GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0);
}
return (0);
}
//******************************************************************************
//
//This is the USCI_A0 interrupt vector service routine.
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_A0_VECTOR)))
#endif
void USCI_A0_ISR(void)
{
switch(__even_in_range(UCA0IV,USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:
RXData = EUSCI_A_UART_receiveData(EUSCI_A0_BASE);
if(!(RXData == TXData)) // Check value
{
while(1);
}
check =1;
break;
case USCI_UART_UCTXIFG:
TXData = TXData+1;
break;
}
}
The interruption is running as expected, but I receive no data on the host PC serial communication. Am I missing something??
Also tried using the MSPWARE example (msp430fr60x7_euscia0_uart_03.c) code with no success. Same happens, registers are configured but no data is received