This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm interesting whether it is possible to use a high-frequency crystal oscillator on pins XIN and XOUT, or is it only supported by a 32,768 Hz clock generator? If there is no such support, is it right that I understand that there is no together support of 24-bit Sigma Delta DACs, 32 KB of RAM and high-frequency crystal oscillator installation in the msp430 processor family.The accuracy of the internal DKO does not match the parameters. Thank you.
Hi Andrey,
can you please elaborate your equation? How do you get to 480kHz?
Andrey Bondarenko said:If so, in the datasheet, the temperature stability is indicated at 0.1% / ° С for 1 MHz, which is 12 MHz, in the temperature range of 40 ° C corresponds to 480 kHz.
Best regards,
Andre
The logic of the calculation is the same, only the temperature range is not 15 ° C, but 50 ° C (-10 ° C ... + 40 ° C).
Andre Frantzke said:The accuracy of this FLL depends on the accuracy of the input source, which can be the XTAL1 32kHz crystal.
Does this mean that if at outputs XIN and XOUT there is 32,768 Hz clock generator, then the accuracy of the DCO will be similar to the accuracy of the crystal oscillator?
Thank you!
**Attention** This is a public forum