Part Number: MSP430I2040
Other Parts Discussed in Thread: MSP430I2041
Tool/software: Code Composer Studio
Hi Sir,
Our customer is using TI EVM430-i2040S with EMDC to test its measurement accuracy,
They have some questions want to know:
1. Will there be a set of current offset settings can provide to adjust it after the EMDC of new version release?
(Due to they observed the current result was not equal to zero when no load, it might have the effect to the precision of test result)
2. Does TI have the test report for EVM430-i2040S (for EMDC version)?
3. They consider to use the transformer to adjust the partial voltage for voltage channel, have any reference document about how to step by step to adjust it?
4. Will the new version EMDC can provide the fine tune function for AC frequency from 45~65 Hz?
5. Is it must have the load when only calibrated the voltage?
6. Have the document to describe that how to calibration the phase step by step?
BTW, they still have the problem about the precision issue as below:
https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/705378
Would you please also help to verify it?
BR
Sam