This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Using CCS Version: 8.0.0.00016
Build and run the Display driver example at
C:\ti\simplelink_msp432e4_sdk_2_20_00_20\examples\rtos\MSP_EXP432E401Y\drivers\display\tirtos\gcc
using the SimpleLink MSP432E4SDK v2.20.0.20 and XDC Tools 3.50.7.20
Teraterm is connected to the the COM port labeled XDS110 Class Application/User UART. The target board has the JP4 and 5 jumpers set to use UART0.
When running the program on a MSP432E401Y LaunchPad, the console output DOES NOT display the Display_printf calls from the Display driver example program (via debugger, one can see that the program is running as expected, ie the Display_printf calls are being made periodically). Also had the same results with the built in Serial Terminal in CCS.
When the exact same program is run on a TIVA 1294 Launchpad, the console output DOES display the data from the Display driver example as expected.
When running the same program on another Windows 10 system using the same version of Teraterm, same CCS, same SDK, the same target board, the console output DOES display the Display_printf data.
Has anyone experienced such issues? It seems like a subtle driver issue on Windows 10, but I am not sure where to start looking. Which files affect the communications on the XDS110 Class Application/User UART? Would much appreciate any insights.
Hi Chris:
I appreciate you keeping an eye on this, as I do need to get this resolved. I have not yet taken a closer look at the drivers on my system to see if there is something I can adjust there. I have had other things that I need to take care of, but I will be getting back to it. It seems to me that there has to be something different about how the XDS110 emulates the comport on the TIVA lauchpad versus the MSP Lauchpad. It seems like there is an awful lot going on in those configuration files, and I can't help but wonder if that has something to do with the issue.
When I am using UART5, I am connecting to the receive and transmit pins of my serial cable to the PC6 and PC7 header pins of the Lauchpad (so as not to use the XDS emulation), and have the UART configuration code set up accordingly.
I don't believe I made any statement that should lead one to assume anything about particular COM port numbers being used on Windows. The com port number on the Windows side is the one which maps to the XDS110 Class Application/User UART as described at the beginning of this thread. In the case of TIVA, it would be the port that maps to the Stellaris. The actual number is not important. I am using a USB-RS232 converter cable to connect the PC to UART5 of the Launchpad.
Edit: July 31 - 2018
I pasted the wrong link above regarding the converter cable we are using. Please refer to the post below dated July 31, 2018 for the correct link to the specification for the converter cable.
Hello Keith:
Thank you for pasting in the relevant information from the link to the spec that I provided. It made me realize that I provided the wrong link (above) to the part we are using. I apologize for the confusion, and extra work this caused you to do!
The correct link to the part we are using is below. We are using the 3V3 part.
https://www.mouser.com/datasheet/2/163/DS_TTL-232R_CABLES-217672.pdf
I will edit the earlier post to refer to this one to help minimize confusion for others.
Paul
Hello Chris:
I connected UART5 to the XDS110 as you described and am still observing the same issue.
To start with, I repeated the experiment above where I ran the program using UART5 with a USB to serial adapter connected to PC6 and PC7 on J1, and observed the console output as expected (this confirms that everything in the software configuration is correct). I then removed the serial adapter from PC6 and PC7, and jumpered PC7 to the TXD pin on the XDS side of J101, and jumpered PC6 to the RXD pin on the XDS side of J101, and removed the jumpers from JP4 and JP5. Ran the same program as before, and NO output was observed on the console. I also tried this on another MSP432 Launchpad and had the same result.
I also uninstalled CCS CCS Version: 8.0.0.00016 and installed the latest Version: 8.1.0.00011 on the off chance that would have some effect. Still the same issue is observed.
Please let me know if there is other information that I can provide that would be helpful. It is important for me to resolve this as soon as possible.
Thank you.
Paul
I got to the bottom of this finally. I had a program named com0com installed on my system which is used for creating virtual serial ports. It was installed quite some time ago, and I forgot that it was there. I spent quite a bit of time today, comparing drivers, etc with other systems to try to see what was different about my system. At some point com0com came to mind. I uninstalled it, and the console started displaying data from the XDS110 as expected. I don't remember which version of com0com I had installed (it was likely either 2.0.0.0 or 2.2.2.0). Perhaps with the latest version of com0com, I would not have these issues, or perhaps there is some setting that needed to be adjusted. Perhaps this not a problem with com0com, but some subtle aspect about how the XDS110 emulates a com port. These details do not matter to me at this point, as I can work around this. At some point I will try to reinstall com0com and see if I can get the XDS110 emulated port to coexist with the com0com virtual ports. The main thing is that I can now fully use the MSP432 Launchpad with my system. This issue can be closed.
**Attention** This is a public forum