This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: I2C Multiple Modules + Sensors

Part Number: MSP432E401Y

Hi, 

I have multiple sensors with the same i2c address and no way to modify that address for them. In the documentation for the msp432e401, it says that there are 10 i2c modules available, but I think they all connect to the same i2c bus? So does this mean that it is not possible to connect these multiple sensors without the use of a mux? Or is there a way to specify the I2C0SDA/SCL pins vs the I2C1SDA/SCL pins? Any help would be appreciated, thanks.

**Attention** This is a public forum