Part Number: MSP430F5438A
Other Parts Discussed in Thread: MSPBSL
I follow the MSPboot code example to design customized boot loader design.
and use CCS5 with lower version compiler for interrupt vector remapping design,
but compiler output wrong tips.
but CCS7 with 16.9.3.LTS compiler version can be ok for this coding.
so I want to know any other way for interrupt remapping to be suitable for different version compiler?
or how to support interrupt remapping in CCS5 for APP code design.
#pragma DATA_SECTION(ProxyVectorTable, ".APP_PROXY_VECTORS")
#pragma RETAIN(ProxyVectorTable)
const uint16_t ProxyVectorTable[] =
{
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(0) RTC
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(1) PORT2
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(2) TIMER2_A1
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(3) TIMER2_A0
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(4) USCI_B1
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(5) USCI_A1
0x4030, (uint16_t)P1_Isr, // APP_PROXY_VECTOR(6) PORT1
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(7) TIMER1_A1
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(8) TIMER1_A0
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(9) DMA
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(10) USB_UBM
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(11) TIMER0_A1
0x4030, (uint16_t)Timer_A, // APP_PROXY_VECTOR(12) TIMER0_A0
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(13) ADC12
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(14) USCI_B0
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(15) USCI_A0
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(16) WDT
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(17) TIMER0_B1
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(18) TIMER0_B0
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(19) COMP_B
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(20) UNMI
0x4030, (uint16_t)Dummy_Isr, // APP_PROXY_VECTOR(21) SYSNMI
};