This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR2433: UART BSL Demo is not working, is there a known issue?

Part Number: MSP-EXP430FR2433
Other Parts Discussed in Thread: MSP430FR2433,

When I attempt to use the UART bootloader demo the target rejects the host and does not boot load.

After reading thru slau550p MSP430FRAM Devices Bootloader document a few times and trying many times to get one MES-EXP430FR2433 launch pad to bootload a second, I have given up.

Short list of the steps I took:

  • I used the provided images in the MSP430FRBoot 1_01_00_00
  • Loaded the UART target into one launch pad, the host boot into another.
  • I crossed the RX line to TX an TX to RX between the two launch pads and a ground line.
  • Verified the target was in Bootloader mode, LED1 and 2 are on.
  • Moved the LED2 of the host to P2.1, (The documentation states to move it to 1.2, but the code seems to use P2.1), either configuration does not seem to make a difference.
  • Press S1 on the host, LED1 would flash and UART character would send at 57600bps.  
  • Start with 0xAA, target would receive 0xAA in the buffer, but my logic analyzer never sees a 0xAA but does see 0x00 acks and 0x80 headers starts.
  • Length, command, and checksums do not seem to be sent correctly, per my logic analyzer.
  • Observed behavior seems to be the same, logic analyzer connected or disconnected, backchannel UARTs connector or disconnected, I have removed the RX/TX jumpers on between the eZ-FET debug prob, no change.

 

Has anyone else been able to get this demo to work on the MSP430FR2433?

 

Thanks

  • Hi Sean,

    Use the same configuration of Host and Target firmware. And try to remove the TXD RXD jumpers connected to the eZ-FET.

    Regards,
    Ling
  • Target Project – MSPBoot_FR2433_UART [BSLBased_dualImg_UART]

    Host Project – MSP-EXP430FR2433_MSPBootHost [ TARGET_FR2433_UART_BSLBASED_DUALIMAGE]

    Using the prebuilt APP1 and APP2. I did not compile and convert to .c files. I am using the supplied .c files.

    #include "TargetApps\App1_FR2433_UART_BSLBased_DualImg_FR2Host.c"
    #include "TargetApps\App2_FR2433_UART_BSLBased_DualImg_FR2Host.c"

    I just tried to roll back the compiler version to 16.9.4 LTS which the project said was used for the build. This did not help. Last time I used 18.1.2 LTS. Jumpers are removed. Behavior has not changed.

    I have also tired to follow the setup in SLAA721b MSP430FRBoot – Main Memory Bootloader and Over-the-Air Updates for
    MSP430™ FRAM Large Memory Model Devices.

    Finally I swapped the Host and Target code in the launch pads. No change.
  • Hi Sean,

    Try the firmware attached.

    @c400
    02 00 10 00 00 00 70 C7 00 00 5E C8 00 00 3A C4 
    00 00 84 C8 00 00 00 00 F2 CE 00 00 06 CD 00 00 
    54 CF 00 00 00 00 06 00 00 00 00 C4 00 00 00 20 
    00 00 24 C4 00 00 10 20 00 00 B2 40 80 5A CC 01 
    D2 43 04 02 D2 C3 02 02 E2 43 04 02 E2 43 02 02 
    92 C3 30 01 1E 14 3D 40 44 28 1E 43 1D 83 0E 73 
    FD 23 0D 93 FB 23 1D 16 03 43 E2 C3 02 02 1E 14 
    3D 40 44 28 1E 43 1D 83 0E 73 FD 23 0D 93 FB 23 
    1D 16 03 43 E2 D3 02 02 1E 14 3D 40 44 28 1E 43 
    1D 83 0E 73 FD 23 0D 93 FB 23 1D 16 03 43 E2 C3 
    02 02 F2 D0 80 00 03 02 F2 D0 80 00 07 02 F2 D0 
    80 00 19 02 F2 D0 80 00 1B 02 F2 F0 7F 00 1D 02 
    8C 00 D8 C6 0D 43 0E 43 B0 13 A4 C6 C2 43 15 20 
    03 43 32 D0 D8 00 03 43 32 C2 03 43 D2 93 15 20 
    F7 23 5F 42 14 20 1F 83 0D 24 1F 83 05 24 3F 80 
    A8 00 05 24 D2 E3 02 02 E2 E3 02 02 05 3C B0 13 
    C0 C6 02 3C D2 E3 02 02 C2 43 15 20 E1 3F 03 43 
    3A 14 8F 00 00 00 9F 00 00 00 04 24 8C 00 00 00 
    B0 13 82 C5 40 18 1A 42 CC 01 40 18 B2 40 80 5A 
    CC 01 8F 00 2E C7 9F 00 32 C7 26 24 89 00 32 C7 
    8F 00 3A C7 D9 0F 20 24 CE 09 0F 19 4E 10 0E 4E 
    0C 4F 0F 19 4F 10 0C 89 0D 4F 0D 7E B0 13 24 C6 
    C8 0C C7 0D 0C 09 7F 4C 4F 0E 4F 05 00 18 5F 4F 
    2E C7 A9 00 04 00 0D 09 4F 13 A9 00 04 00 18 83 
    07 73 F0 23 08 93 EE 23 7A C2 3A D0 08 5A 40 18 
    82 4A CC 01 B0 13 EC C6 8F 00 00 00 9F 00 00 00 
    09 24 8A 00 00 00 03 3C 6A 13 AA 00 04 00 9A 00 
    00 00 FA 23 37 16 10 01 2A 14 C9 0C 18 49 02 00 
    0A 43 2F 3C CC 0A 0D 43 3E 40 0C 00 0F 43 B0 13 
    80 C6 0F 18 4D 5D 00 18 4D DC ED 09 CC 0D 1E 4C 
    0C 00 1F 4C 0E 00 3D 0C 04 00 3B 0C 08 00 CC 0B 
    0F 93 12 20 0E 93 10 20 8F 00 2E C7 9F 00 32 C7 
    0F 24 6F 4D 4F 06 00 18 5F 4F 2E C7 AD 00 01 00 
    CC 0D CD 0B 4F 13 02 3C B0 13 32 C6 18 49 02 00 
    1A 53 0A 98 CF 2B 28 16 10 01 5D 01 5C 00 5D 01 
    5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 
    5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 
    5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 
    5C 00 5D 01 5C 00 10 01 1A 14 C9 0C 0F 93 02 20 
    0E 93 0D 24 0A 43 0B 43 A9 00 01 00 F9 4D FF FF 
    1A 53 0B 63 0B 9F F8 2B 02 20 0A 9E F5 2B 19 16 
    10 01 1F 4C 01 00 1E 4C 03 00 0E 93 02 20 0F 93 
    09 24 AD 00 01 00 CD 43 FF FF 1F 83 0E 73 F9 23 
    0F 93 F7 23 10 01 02 12 32 C2 03 43 82 4C D0 04 
    82 4D D2 04 82 4E E0 04 82 4F E2 04 1C 42 E4 04 
    1D 42 E6 04 32 41 03 43 10 01 60 0C 08 20 60 0D 
    0C 20 60 0E 10 20 8C 00 08 20 1F 42 7A FF 4F 13 
    92 D3 1A 05 10 01 B2 40 DE C0 00 20 D2 D3 02 20 
    32 C2 03 43 B2 40 04 A5 20 01 FF 3F 03 43 C2 4C 
    14 20 D2 43 15 20 10 01 03 43 FF 3F 03 43 1C 43 
    10 01 10 01 81 00 00 30 B0 13 E8 C6 0C 93 02 24 
    B0 13 DA C4 0C 43 B0 13 04 C4 B0 13 E2 C6 4F 14 
    1F 42 7C FF 4F 13 B1 C0 D0 00 14 00 4B 16 00 13 
    C2 43 1D 02 E2 E3 02 02 00 13 FF 3F 03 43 00 00 
    0E 00 00 00 5C C6 00 00 28 C7 00 00 08 20 00 00 
    B2 40 80 5A CC 01 D2 D3 04 02 D2 D3 02 02 92 C3 
    30 01 1E 14 3D 40 44 28 1E 43 1D 83 0E 73 FD 23 
    0D 93 FB 23 1D 16 03 43 D2 C3 02 02 1E 14 3D 40 
    44 28 1E 43 1D 83 0E 73 FD 23 0D 93 FB 23 1D 16 
    03 43 D2 D3 02 02 1E 14 3D 40 44 28 1E 43 1D 83 
    0E 73 FD 23 0D 93 FB 23 1D 16 03 43 D2 C3 02 02 
    F2 D0 80 00 03 02 F2 D0 80 00 07 02 F2 D0 80 00 
    19 02 F2 D0 80 00 1B 02 F2 F0 7F 00 1D 02 B2 40 
    10 00 82 03 B2 40 E7 03 92 03 B2 40 10 01 80 03 
    03 43 32 D0 D8 00 03 43 03 43 0C 43 10 01 B2 40 
    DE C0 00 20 D2 D3 02 20 32 C2 03 43 B2 40 04 A5 
    20 01 FF 3F 03 43 03 43 FF 3F 03 43 1C 43 10 01 
    81 00 00 30 B0 13 C0 C4 0C 43 B0 13 04 C4 B0 13 
    BA C4 4F 14 C2 43 1D 02 B0 13 A2 C4 4B 16 00 13 
    D2 E3 02 02 92 C3 82 03 00 13 FF 3F 03 43 D6 C4 
    EE C4 EE C4 EE C4 EE C4 EE C4 EE C4 EE C4 EE C4 
    EE C4 EE C4 EE C4 EE C4 EE C4 EE C4 E4 C4 EE C4 
    EE C4 C4 C4 1A C7 24 C7 24 C7 24 C7 24 C7 08 C7 
    24 C7 24 C7 24 C7 24 C7 24 C7 24 C7 24 C7 24 C7 
    24 C7 24 C7 24 C7 24 C7 EE C6 00 C4 03 C4 FF D9 
    04 C4 DA D9 EE 00 26 00 04 C4 DA D9 36 03 26 00 
    0A 14 F1 03 B2 40 80 5A CC 01 B2 40 06 00 82 01 
    B2 40 00 01 88 01 8C 00 B0 C8 8D 00 B4 C8 8E 00 
    00 20 6F 43 B0 13 0A CC 82 4C 12 20 8C 00 B8 C8 
    8D 00 BC C8 8E 00 08 20 B0 13 0A CC 82 4C 14 20 
    C2 43 11 20 C2 43 10 20 B0 13 16 CF F2 D2 03 02 
    D2 C3 02 02 D2 D3 04 02 F2 D2 07 02 F2 D2 19 02 
    F2 C2 1D 02 F2 D2 1B 02 E2 D3 03 02 E2 D3 05 02 
    92 C3 30 01 F2 C2 1D 02 03 43 32 D0 18 00 03 43 
    32 C2 03 43 C2 93 11 20 F5 27 D2 E3 02 02 1E 14 
    3D 40 64 C9 3E 42 1D 83 0E 73 FD 23 0D 93 FB 23 
    1D 16 03 43 D2 E3 02 02 1E 14 3D 40 64 C9 3E 42 
    1D 83 0E 73 FD 23 0D 93 FB 23 1D 16 03 43 D2 E3 
    02 02 1E 14 3D 40 64 C9 3E 42 1D 83 0E 73 FD 23 
    0D 93 FB 23 1D 16 03 43 D2 E3 02 02 B0 13 8E CF 
    4C 93 C8 27 7C 40 AA 00 B0 13 C8 CE 0D 14 3D 40 
    27 68 1D 83 FE 23 0D 16 03 43 B0 13 82 CF 7C 40 
    19 00 B0 13 22 CE 4C 4C 3C F0 F0 FF 3C 90 A0 00 
    87 20 7C 40 15 00 B0 13 22 CE 4C 93 AB 23 C2 93 
    10 20 2A 24 4A 43 6A 93 19 2C 4F 4A 5F 02 40 18 
    1F 4F BC C8 81 43 00 00 4E 4A 5E 02 40 18 1C 4E 
    B8 C8 0D 43 4E 4A 5E 06 00 18 5E 4E 08 20 B0 13 
    F2 CA 4C 93 03 20 5A 53 6A 93 E7 2B 2F 43 81 43 
    00 00 40 18 1C 42 AA C8 0D 43 8E 00 14 20 B0 13 
    F2 CA 4C 93 7F 23 29 3C 4A 43 6A 93 19 2C 4F 4A 
    5F 02 40 18 1F 4F B4 C8 81 43 00 00 4E 4A 5E 02 
    40 18 1C 4E B0 C8 0D 43 4E 4A 5E 06 00 18 5E 4E 
    00 20 B0 13 F2 CA 4C 93 03 20 5A 53 6A 93 E7 2B 
    2F 43 81 43 00 00 40 18 1C 42 AA C8 0D 43 8E 00 
    12 20 B0 13 F2 CA 4C 93 55 23 7C 40 1C 00 B0 13 
    22 CE 1E 14 3D 40 64 C9 3E 42 1D 83 0E 73 FD 23 
    0D 93 FB 23 1D 16 03 43 D2 E3 02 02 1E 14 3D 40 
    64 C9 3E 42 1D 83 0E 73 FD 23 0D 93 FB 23 1D 16 
    03 43 D2 E3 02 02 1E 14 3D 40 64 C9 3E 42 1D 83 
    0E 73 FD 23 0D 93 FB 23 1D 16 03 43 D2 E3 02 02 
    C2 43 11 20 D2 E3 10 20 C2 93 11 20 23 27 2D 3F 
    03 43 5A 14 B1 00 0C 00 CA 0F C5 0E C8 0C C7 0D 
    19 41 28 00 09 93 02 20 0A 93 37 24 09 93 05 20 
    3A 90 11 00 02 2C C6 0A 02 3C 36 40 10 00 F1 40 
    10 00 02 00 71 05 06 00 CF 06 6F 52 C1 4F 01 00 
    C1 47 05 00 CF 08 8F 10 C1 4F 04 00 C1 48 03 00 
    CC 01 B0 13 7C CD 81 4C 0A 00 CC 01 B0 13 82 CB 
    27 93 05 28 03 20 38 90 00 3F 01 28 03 43 B0 13 
    9A CE 4C 93 0A 20 0A 86 09 73 08 56 07 63 0F 46 
    E5 0F 09 93 CB 23 0A 93 C9 23 A1 00 0C 00 55 16 
    10 01 B1 00 0E 00 CD 0C CC 01 3E 40 0C 00 0F 43 
    B0 13 5E CE 7C 40 80 00 B0 13 C8 CE 5C 41 01 00 
    B0 13 C8 CE 5C 41 02 00 B0 13 C8 CE E1 93 01 00 
    1B 28 5C 41 03 00 B0 13 C8 CE 5C 41 04 00 B0 13 
    C8 CE 5C 41 05 00 B0 13 C8 CE 0D 43 08 3C 0F 4D 
    00 18 5F 51 06 00 6C 4F B0 13 C8 CE 1D 53 5F 41 
    01 00 2F 82 0D 9F F3 2B D1 41 0A 00 0D 00 5C 41 
    0D 00 B0 13 C8 CE D1 41 0B 00 0C 00 5C 41 0C 00 
    B0 13 C8 CE A1 00 0E 00 10 01 3A 14 B2 43 C4 01 
    40 18 18 42 AC C8 40 18 82 98 AE C8 34 28 49 43 
    01 3C 59 53 49 9F 26 2C 4B 49 5B 02 4B 0E 4B 0D 
    EB 0C 28 9B F6 2B 4B 49 5B 02 4B 0E 4B 0D EB 0C 
    4A 49 5A 02 4A 0E 4A 0D EA 0D 2A 4A 2A 5B 08 9A 
    E8 2F 4B 49 5B 06 4B 0E 4B 0D EB 0E 4A 49 5A 02 
    4A 0E 4A 0D EA 0C C7 08 27 8A 0A 47 00 18 6A 5B 
    E2 4A C2 01 49 9F 02 20 F2 43 C2 01 18 53 40 18 
    82 98 AE C8 CC 2F 1C 42 C4 01 37 16 10 01 3A 14 
    40 18 1A 42 CC 01 40 18 B2 40 80 5A CC 01 8F 00 
    18 C4 9F 00 24 C4 25 24 89 00 2A C4 8F 00 3A C4 
    D9 0F 1F 24 CE 09 0F 19 4E 10 0E 4E 0C 4F 0F 19 
    4F 10 0C 89 0D 4F 0D 7E B0 13 14 CE C8 0C C7 0D 
    0C 09 7F 4C 5F 06 00 18 5F 4F 18 C4 A9 00 04 00 
    0D 09 4F 13 A9 00 04 00 18 83 07 73 F1 23 08 93 
    EF 23 7A C2 3A D0 08 5A 40 18 82 4A CC 01 B0 13 
    96 CF 37 16 10 01 2A 14 78 4C 09 43 14 3C 0B 4B 
    CE 0D FE 0B BE 00 01 00 AD 00 01 00 FD 4E FF FF 
    1F 83 FA 23 04 3C AD 00 01 00 FD 4C FF FF 58 03 
    19 53 39 92 E9 37 18 B3 F6 23 7B 4C 7F 4C CE 0B 
    5E 0E CB 0F 5B 0F 3B F0 0F 00 0B DE 3F F0 0F 00 
    3F 50 03 00 3F 90 12 00 0C 20 7E 4C 3E B0 80 00 
    07 24 7A 4C 3E F0 7F 00 4A 4A 46 18 0A 5A 0E DA 
    0F 5E 3B 90 FF 0F CB 23 28 16 10 01 B1 00 0C 00 
    CD 0C CC 01 3E 40 0C 00 0F 43 B0 13 5E CE B2 43 
    C4 01 CE 01 EE 03 5C 41 01 00 0F 43 4D 4C 0F 9D 
    1C 2C 2F 92 12 28 2F 92 07 24 CD 0F 2D 82 0D 4D 
    ED 0E E2 4D C2 01 0D 3C 3E 01 06 00 CD 0F 2D 82 
    0D 4D ED 0E E2 4D C2 01 04 3C 0D 4F ED 0E E2 4D 
    C2 01 1F 53 4D 4C 0F 9D E4 2B 1C 42 C4 01 A1 00 
    0C 00 10 01 5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 
    5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 
    5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 
    5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 5D 01 5C 00 
    10 01 0A 14 B1 00 0C 00 CA 0C F1 40 80 00 00 00 
    C1 4A 02 00 D1 43 01 00 CC 01 B0 13 7C CD 81 4C 
    0A 00 CC 01 B0 13 82 CB 7A 90 1C 00 03 24 B0 13 
    9A CE 01 3C 4C 43 A1 00 0C 00 0A 16 10 01 2A 14 
    0F 93 02 20 0E 93 17 24 09 43 08 43 CB 08 0F 18 
    4B 5B 00 18 4B D9 EB 0D CA 08 0F 18 4A 5A 00 18 
    4A D9 EA 0C EA 4B 00 00 19 53 08 63 08 9F EE 2B 
    02 20 09 9E EB 2B 28 16 10 01 3E 40 60 E3 3F 40 
    16 00 92 B3 1C 05 06 20 1E 83 0F 73 3F 93 F9 23 
    3E 93 F7 23 0F 93 02 20 0E 93 04 24 1C 42 0C 05 
    4C 4C 01 3C 7C 43 10 01 3E 40 60 E3 3F 40 16 00 
    A2 B3 1C 05 06 20 1E 83 0F 73 3F 93 F9 23 3E 93 
    F7 23 0F 93 02 20 0E 93 03 24 4C 4C 82 4C 0E 05 
    10 01 1F 4C 01 00 1E 4C 03 00 0E 93 02 20 0F 93 
    09 24 AD 00 01 00 CD 43 FF FF 1F 83 0E 73 F9 23 
    0F 93 F7 23 10 01 B2 40 81 00 00 05 F2 40 30 00 
    0A 02 F2 F0 CF 00 0C 02 B2 42 06 05 B2 40 A1 F7 
    08 05 D2 C3 00 05 10 01 81 00 00 30 B0 13 92 CF 
    0C 93 02 24 B0 13 8E CC 0C 43 B0 13 C0 C8 1C 43 
    B0 13 88 CF CF 0C CC 0D CD 0F AD 00 05 00 1E 4F 
    01 00 1F 4F 03 00 80 00 5E CE F2 C2 1D 02 D2 43 
    11 20 B1 C0 10 00 00 00 00 13 32 D0 10 00 FD 3F 
    03 43 92 C3 1C 05 10 01 03 43 FF 3F 03 43 5C 43 
    10 01 1C 43 10 01 10 01 
    @ff80
    FF FF FF FF FF FF FF FF 
    @ffda
    6A CF 7A CF 7A CF 7A CF 7A CF 7A CF 7A CF 7A CF 
    7A CF 7A CF 7A CF 7A CF 7A CF 7A CF 7A CF 7A CF 
    7A CF 7A CF 38 CF 
    q
    

    @f000
    6A 14 B0 13 DC F0 67 4B 47 47 06 43 2D 3C C9 0E 
    CA 0F 09 88 0A 73 19 83 0A 73 C5 09 C8 0A 19 53 
    0A 63 0F 18 48 58 00 18 48 D5 65 48 C4 0E C8 0F 
    1E 53 0F 63 0F 18 48 58 00 18 48 D4 C8 45 00 00 
    1B 83 EB 23 0D 3C B0 13 DC F0 6A 4B C9 0E CB 0F 
    1E 53 0F 63 0F 18 4B 5B 00 18 4B D9 CB 4A 00 00 
    57 03 16 53 36 92 CD 37 17 B3 ED 23 B0 13 DC F0 
    68 4B 48 48 B0 13 DC F0 6B 4B 4B 4B CA 08 5A 0E 
    C8 0B 58 0F 38 F0 0F 00 08 DA 3B F0 0F 00 3B 50 
    03 00 3B 90 12 00 1D 20 C9 0C CA 0D 1C 53 0D 63 
    0F 18 4A 5A 00 18 4A D9 6A 4A 4A 4A 3A B0 80 00 
    0F 24 C5 0C C9 0D 1C 53 0D 63 0F 18 49 59 00 18 
    49 D5 69 49 3A F0 7F 00 49 49 46 18 09 59 0A D9 
    0B 5A 38 90 FF 0F 9B 23 64 16 10 01 CA 0C CB 0D 
    1C 53 0D 63 0F 18 4B 5B 00 18 4B DA 10 01 C2 93 
    1C 20 10 20 F2 40 55 00 21 20 7C 90 80 00 52 24 
    F2 D2 20 20 F2 40 51 00 21 20 7C 90 AA 00 4A 24 
    03 43 48 3C D2 93 1C 20 35 24 5F 42 1D 20 2F 53 
    5E 42 1C 20 0E 9F 27 38 5E 42 1C 20 0E 9F 1F 24 
    5F 42 1D 20 3F 50 03 00 5E 42 1C 20 0E 9F 32 20 
    4C 4C 47 18 0C 5C 82 5C 1E 20 5D 42 1D 20 0E 43 
    3C 40 08 20 3F 43 B0 13 2C F7 1C 92 1E 20 03 20 
    E2 D3 20 20 1F 3C F2 40 52 00 21 20 19 3C 4C 4C 
    82 4C 1E 20 17 3C 5F 42 1C 20 3F 50 08 20 CF 4C 
    FE FF 10 3C C2 4C 1D 20 4C 93 07 24 7C 90 15 00 
    09 28 F2 40 54 00 21 20 03 3C F2 40 53 00 21 20 
    F2 D2 20 20 F2 B2 20 20 03 20 D2 53 1C 20 10 01 
    5C 42 21 20 B0 13 8C F7 C2 43 20 20 C2 43 1C 20 
    10 01 4A 14 C6 0E CF 0D CA 0C 6E 4A 3E 80 10 00 
    28 24 2E 83 0F 24 3E 80 03 00 54 24 2E 82 4E 24 
    3E 80 03 00 02 20 6C 43 52 3C F6 40 C6 00 00 00 
    5C 43 4D 3C 5C 4A 02 00 0D 43 B0 13 3A F6 5E 4A 
    01 00 0F 43 5B 4A 03 00 3B F0 0F 00 0F 5B 0C 5E 
    0D 6F B0 13 92 F2 4C 93 37 24 F6 40 C5 00 00 00 
    35 3C 5C 4A 02 00 0D 43 B0 13 3A F6 58 4A 01 00 
    09 43 5E 4A 03 00 3E F0 0F 00 09 5E 08 5C 09 6D 
    B2 40 01 A5 60 01 C7 0F 67 82 0E 24 2A 52 47 47 
    CC 08 CD 09 18 53 09 63 6E 4A B0 13 5E F5 4C 93 
    05 20 1A 53 17 83 F4 23 0F 43 02 3C 3F 40 C5 00 
    B2 40 03 A5 60 01 C6 4F 00 00 08 3C F6 40 A1 00 
    00 00 04 3C B0 13 A2 F7 C6 43 00 00 4C 43 46 16 
    10 01 0D 93 03 20 3C 90 00 C4 14 28 3E 40 FF D9 
    0F 43 0F 9D 03 28 07 20 0E 9C 05 2C 0D 93 03 20 
    3C 90 00 DA 07 28 3E 40 FF EF 0F 9D 03 28 04 20 
    0E 9C 02 2C 5C 43 10 01 B0 13 54 F7 B2 40 00 A5 
    60 01 CB 0C CE 0D 3B 50 00 02 0E 63 09 3C CF 0D 
    0F 18 4F 5F 00 18 4F DC BF 43 00 00 2C 53 0D 63 
    0D 9E F5 2B 02 20 0C 9B F2 2B B2 40 03 A5 60 01 
    4C 43 10 01 0F 43 D2 B3 02 20 05 24 B2 90 DE C0 
    00 20 01 20 1F 43 0D 14 3D 40 02 0D 1D 83 FE 23 
    0D 16 F2 B0 80 FF 01 02 01 20 1F 43 82 43 00 20 
    C2 43 02 20 0F 93 19 20 4C 43 B0 13 CC F4 1C 93 
    12 24 5C 43 B0 13 CC F4 1C 93 0F 20 4C 43 B0 13 
    22 F4 B0 13 CA F3 4C 43 B0 13 CC F4 1C 93 05 20 
    5C 43 B0 13 22 F4 1C 43 10 01 0C 43 10 01 B2 40 
    80 5A CC 01 F2 D0 80 00 03 02 F2 D0 80 00 07 02 
    92 C3 30 01 B2 40 06 00 82 01 B2 40 00 01 88 01 
    82 43 8A 01 B0 13 04 F3 1C 93 03 20 1F 42 FE D9 
    4F 13 B0 13 76 F7 D2 D3 04 02 E2 D3 04 02 D2 D3 
    02 02 E2 D3 02 02 B0 13 1C F5 B0 13 98 F6 6C 93 
    FA 23 B0 13 CC F6 F7 3F 03 43 1A 14 21 82 3F 40 
    00 C4 71 0F 00 00 39 40 FF D9 0A 43 1A 91 02 00 
    1D 28 02 20 29 91 1A 28 2C 41 1D 41 02 00 B0 13 
    54 F7 0F 18 4D 5D 00 18 4D DC 6E 4D 2C 41 1D 41 
    02 00 B0 13 78 F4 03 43 91 53 00 00 81 63 02 00 
    1A 91 02 00 03 28 E8 23 29 91 E6 2F 21 52 19 16 
    10 01 1A 14 C9 0C B2 40 00 A5 60 01 3A 40 FF D9 
    0B 43 3E 40 00 C4 0F 43 0B 9F 19 28 02 20 0A 9E 
    16 28 49 93 03 20 CD 0F CC 0E 04 3C CC 0E CD 0F 
    B0 13 54 F7 0F 18 4D 5D 00 18 4D DC BD 43 00 00 
    2E 53 0F 63 0B 9F 03 28 EC 23 0A 9E EA 2F B2 40 
    03 A5 60 01 19 16 10 01 0A 14 B2 40 00 A5 60 01 
    CF 0D 0F 18 4F 5F 00 18 4F DC CF 4E 00 00 3A 40 
    88 D9 0B 43 0D 9B 15 28 02 20 0C 9A 12 28 3F 40 
    FE D9 2F 83 0D 93 0D 20 0C 9F 0B 2C 0C 8A 0D 7B 
    3C 50 88 FF 0D 63 0F 18 4D 5D 00 18 4D DC CD 4E 
    00 00 B2 40 03 A5 60 01 0A 16 10 01 4C 93 04 20 
    B2 93 FE D9 1F 24 20 3C B2 43 C4 01 3B 40 FD 15 
    0C 43 0C 93 02 20 0B 93 0D 24 3D 40 03 DA 0E 43 
    0F 43 F2 4D C2 01 1E 53 0F 63 0F 9C FA 2B 02 20 
    0E 9B F7 2B 1E 42 C4 01 82 4E 22 20 3F 40 00 DA 
    2E 9F 02 24 0C 43 10 01 1C 43 10 01 21 83 1F 42 
    1C 05 4F 4F 5F B3 0E 20 6F B3 17 24 1F 42 04 20 
    3F 0F 04 00 DF 03 11 24 CC 01 4F 13 6F 41 82 4F 
    0E 05 0B 3C 1F 42 0C 05 C1 4F 00 00 1F 42 04 20 
    0F 0F DF 03 02 24 6C 41 4F 13 21 53 10 01 0D 93 
    03 20 3C 90 00 C4 14 28 3B 40 FF D9 0F 43 0F 9D 
    03 28 07 20 0B 9C 05 2C 0D 93 03 20 3C 90 00 DA 
    07 28 3B 40 FF EF 0F 9D 03 28 04 20 0B 9C 02 2C 
    5C 43 10 01 B0 13 54 F7 B0 13 78 F4 4C 43 10 01 
    0A 14 1A 41 08 00 1B 41 0A 00 0F 18 4D 5D 00 18 
    4D DC 0F 18 4F 5F 00 18 4F DE 0B 93 02 20 0A 93 
    0D 24 0C 43 0E 43 AD 00 01 00 FD 4F FF FF 1C 53 
    0E 63 0E 9B F8 2B 02 20 0C 9A F5 2B 0A 16 10 01 
    0A 14 1C 53 0D 63 0F 18 4D 5D 00 18 4D DC 2C 4D 
    1B 4D 02 00 0B 93 02 20 0C 93 0F 24 CA 0E CD 0F 
    1E 53 0F 63 0F 18 4D 5D 00 18 4D DA CD 43 00 00 
    1C 83 0B 73 F3 23 0C 93 F1 23 0A 16 10 01 5C 02 
    0D 6D 5C 02 0D 6D 5C 02 0D 6D 5C 02 0D 6D 5C 02 
    0D 6D 5C 02 0D 6D 5C 02 0D 6D 5C 02 0D 6D 5C 02 
    0D 6D 5C 02 0D 6D 5C 02 0D 6D 5C 02 0D 6D 5C 02 
    0D 6D 5C 02 0D 6D 5C 02 0D 6D 10 01 0A 14 21 82 
    CB 0C CA 0D CC 0E CD 0F CE 0B CF 0A CA 0E CB 0F 
    1A 53 0B 63 0F 18 4B 5B 00 18 4B DA 1A 4B 02 00 
    A1 4B 00 00 81 4A 02 00 3E 50 05 00 0F 63 B0 13 
    A0 F5 21 52 0A 16 10 01 0A 14 E2 B3 20 20 02 20 
    0A 43 11 3C 3C 40 08 20 5D 42 1D 20 3E 40 21 20 
    B0 13 C2 F1 4A 4C 5C 42 21 20 B0 13 8C F7 C2 43 
    1C 20 C2 43 20 20 CC 0A 0A 16 10 01 B2 40 4D 5A 
    CC 01 5C 43 B0 13 CC F4 1C 93 0D 20 4C 43 B0 13 
    22 F4 B0 13 CA F3 4C 43 B0 13 CC F4 1C 93 03 20 
    5C 43 B0 13 22 F4 B2 40 04 A5 20 01 10 01 B2 40 
    81 00 00 05 F2 F0 CF 00 0C 02 F2 D0 30 00 0A 02 
    F2 42 06 05 C2 43 07 05 B2 40 A1 F7 08 05 92 C3 
    00 05 82 4C 04 20 82 43 03 20 10 01 B2 43 C4 01 
    0E 93 02 20 0D 93 0B 24 0B 43 0F 43 F2 4C C2 01 
    1B 53 0F 63 0F 9E FA 2B 02 20 0B 9D F7 2B 1C 42 
    C4 01 10 01 31 82 81 4C 04 00 81 4D 06 00 3C 50 
    00 16 0D 63 81 4C 00 00 81 4D 02 00 2C 41 1D 41 
    02 00 31 52 10 01 C2 43 20 20 C2 43 1C 20 F2 40 
    55 00 21 20 3C 40 A8 F7 80 00 FE F6 A2 B3 1C 05 
    FD 27 4C 4C 82 4C 0E 05 10 01 31 40 00 30 B0 13 
    6E F3 5C 43 80 00 22 F4 EE F0 00 00 00 00 00 00 
    00 00 00 00 E0 F5 00 00 00 F0 00 00 5C F6 00 00 
    00 00 1A 00 00 00 01 03 00 00 FF F0 C0 F7 00 00 
    08 20 00 00 C6 F7 00 00 22 20 00 00 
    @ff7a
    FE F6 1C F5 8C F7 
    @fffe
    9A F7 
    q
    

  • I was able to get the demo to work from the images you sent. I ended up taking a brand new MSP-EXP430FR2433 launchpad, loaded the target file you linked.   Now I am able to run thru the demo described in slaa721b.

    Only a couple issues I found from that from the demo in SLAA721b as they pertain to the files you linked.

     Section 5.3 slaa721b.pdf

     I skipped section 1 – 4, because I loaded the images you provided.

     Steps 5 thru 8 worked normally

    Step 9 has a discrepancy.

    9. States, with the target in bootloader press S2 on host to send APP2.   S2 has no effect. Pressing S1 when LED 1 is solid during this step sends App2.

    Completed thru step 11.

     Also, there is a Note at the end of this section stating:

     Due to a pin conflict on the MSP-EXP430FR2433, disconnected LED2 from P1.1 by removed the jumper and physically wire to P1.2 instead.

     This does not seem to do anything, and it also does not state if this is the Target or Host or both boards need this done. I successfully ran the demos leaving the LED 2 jumper in place.

    Question:

    Did you do anything different from the projects in the MSP430FRBoot_1_01_00_00.zip files and instruction using SLAA721b?

    Thanks

    Sean

  • Hi Sean,

    I didn't do anything different from the project. Please find my projects attached.

    MSPBoot_FR2433_UART.zipMSP-EXP430FR2433_MSPBootHost.zip

    Ling

  • Hi Sean,

    Any update from your side?

    Ling
  • I have been able to use the firmware images you provided as well as the BSL Scripter software to load various images on two different MSP430FR Devices.  I am still planning on trying to rebuild them from the projects to see if I can learn what I did that was different.  But for now I have been able to confirm that the boot loader and my hardware is working, that was the original issue.


    Thank you,


    Sean

**Attention** This is a public forum