This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430AFE253: Microcontroller stop work

Part Number: MSP430AFE253

Hi,

I am using MSP430AFE253, MSP-FET-430UIF, SBW protocol and CCS v7.2.

My problem is: Some time ago I received some microcontrollers that I can flash once, when I tried to flash again they return "unknown device", I tried everything (hardware double checked): the microcontrollers died. I replaced the microcontroller and got the same behavior.
The ""solution"" was to change the RST capacitor to 1pF in my fourth microcontroller. I do not understand why, but it works on this microcontroller, the other three microcontrollers I've used have died.

Today I was debugging my project and realized that the DCO frequency was not setting as I expected in my code. But when I used the standard dco frequency, the program works fine. So I decided to debug step by step to see why my DCO setup did not work. Then, after the DCO frequency registers (DCO and BCSCTL1), an error called "can't single step target program: Could not single step device" occurs and after that, I received "unknown device error" for further flashes

I have not changed anything on the hardware, it's the same before the error "can't single step target program: Could not single step device.". I thing the microcontroller died as the others.

What is going on? I do not have replacement microcontroller.

Sorry for bad english.

#include <msp430afe253.h>
#include "math.h"
#include <stdlib.h>

#define iddle '0'
#define ready '1'
#define id '2'
#define get '3'
#define set '4'
#define reset '5'

#define gain_1 '6'
#define gain_2 '7'
#define gain_3 '8'
#define gain_4 '9'
//#define gain_end 's'
#define TEST 'U'
#define FREQUENCY_AMOUNT 23


#define SAMPLE_CYCLE 65
#define kv 0.005967907402
#define ka 0.0001021671827
#define kw 0.000007716049383
#define TIMER_FREQ_DIVIDER 8
#define UART_CALC_CONST 8
#define BAUDRATE 9600
//#define kv 1
//#define ka 1

//Variables

// Only for debugging Labview//
union wave
{
int all_wave;
char pt_wave[2];

};

union wave voltage_wave;
union wave current_wave;
//----------------------------//
union VI
{
float all_VI;
char pt_VI[4];
};

union VI voltage;
union VI current;
union VI energy;
union VI ActPower;
union VI ReactEnergy;
union VI ReactPower;
union VI PowerFactor;

union BaudrateRegister
{
unsigned int brdiv;
short int p_brdiv[2];
};

union BaudrateRegister ubr;

unsigned char uart_state;
unsigned char gain_state;
unsigned char bufferRX;
unsigned char send_relay = 'N';

short int R0 = 0, R1 = 0;
short int Port_flag = 1;
short int s_count = 0, freq_adjust_flag = 0;
short int idx = 0, send = 0;
const short int LimR0[23] = {42,41,40,39,38,37,36,35,34,33,32,31,30,29,28,27,26,25,24,23,22,21,20};
const short int LimR1[23] = {21,21,20,20,19,19,18,18,17,17,16,16,15,15,14,14,13,13,12,12,11,11,10};

int frequency;
int I_buffer[59], V_buffer[59];
int I_AD_RESULT, V_AD_RESULT;
int I_buffer_accum = 0, V_buffer_accum = 0;

signed long int V1_avg = 0, I1_avg = 0;
signed long long int V_acum=0, I_acum=0, V_operand = 0, I_operand = 0;
signed long long int P_acum = 0;

float V_rms = 0, I_rms = 0;
float PF = 0, S = 0, P = 0, E = 0, React_E = 0;
float argument = 0;

unsigned int count_final = 0, count_initial = 0, count_result = 0;
unsigned int ubrs = 0;
float brdiv_rest = 0,count_frequency = 0;
//

//Functions
void clock_init();
void sd_init();
void port_init();
void UART_init();
void measurement();
void calculate();
void command(unsigned char);
void send_param(int f);
void relay(unsigned char);
int PWM_adjust();
void PWM(int j, int s);
void configura_timer(short int s);
void calcula_baudrate();
//


void clock_init()
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
// MCLK = ~1MHz
BCSCTL1 &= ~XT2OFF; // XT2 is on
BCSCTL3 = XT2S_2; //3- to 16-MHz crystal or resonator
do
{
IFG1 &= ~OFIFG;
__delay_cycles(100); //100us em ~1MHz
}
while(IFG1 & OFIFG);
BCSCTL2 = SELM_2; // Select MCLK: SELM_2 -> XT2CLK when XT2 oscillator present on-chip
//MCLK = 12MHz from crystal

DCOCTL = DCO0 + DCO1 + DCO2; //DCO = 7, MODx = 0
BCSCTL1 |= RSEL0 + RSEL1 + RSEL2 + RSEL3; // RSELx = 15
//SMCLK = ~20MHz
}

void port_init()
{
P2DIR |= BIT0; //LED
// P2OUT &= ~BIT0; //LED
// P2OUT |= BIT0;
// P1SEL |= BIT0; // SMCLK Pin Function
// P1SEL2 |= BIT0;

P1DIR |= BIT0 | BIT1; // P1.0 = Relay, P1.1 = PWM
P1SEL |= BIT1 | BIT3 | BIT4; //P1.1 = TA1, P1.3,1.4 = USART0 TXD/RXD
P1OUT &= ~BIT0;
// P1OUT |= BIT0;

}

void calcula_baudrate()
{
float aux = 0;
float auxf = 0;
P2OUT |= BIT0;
count_initial = TA0R;
__delay_cycles(120000);
P2OUT &= ~BIT0;
count_final = TA0R;
CCTL0 &= ~CCIE;
count_result = count_final - count_initial;

count_frequency = count_result * TIMER_FREQ_DIVIDER;

auxf = count_frequency / BAUDRATE;
ubr.brdiv = (int)auxf;
brdiv_rest = auxf - ubr.brdiv;
aux = brdiv_rest * UART_CALC_CONST;
ubrs = roundf(aux);
if (ubrs < aux)
{
ubrs += 1;
}

}

void UART_init()
{
ME1 |= UTXE0 + URXE0; // Enable USART0 TXD/RXD
U0CTL |= CHAR + SWRST; // 8-bit character, USART in reset state
U0TCTL |= SSEL1; // UCLK= MCLK
U0BR0 = ubr.p_brdiv[0]; // 21.71MHz 9600 b/s +significativo
U0BR1 = ubr.p_brdiv[1]; // 21.71MHz 9600 b/s - significativo
U0MCTL = ubrs; // 21.71MHz 9600 b/s modulation
U0CTL &= ~SWRST; // 8-bit character, USART ready
IE1 = URXIE0; // Enable USART0 RX interrupt
}

void sd_init()
{
//Frequência de amostragem =
volatile unsigned int j;

SD24CTL |= SD24XDIV_1 | SD24DIV_2 | SD24SSEL_0 | SD24REFON; // clock divider = 12 | clock source select = MCLK | Reference generator on = 1

//Configure channel 0 - Voltage

// SD24CCTL0 = SD24XOSR | SD24GRP | SD24IE | SD24DF; //Enable Interrupt, data format = 2's complement, oversampling = 512
SD24CCTL0 = SD24GRP | SD24IE | SD24DF; //Enable Interrupt, data format = 2's complement, oversampling = 256
SD24INCTL0 = SD24GAIN_2;

//Configure Channel 1 - Current
// SD24CCTL1 |= SD24XOSR | SD24IE | SD24DF; // //Enable Interrupt, data format = 2's complement, oversampling = 512
SD24CCTL1 |= SD24IE | SD24DF; // //Enable Interrupt, data format = 2's complement, oversampling = 256
SD24INCTL1 = SD24GAIN_4;

for (j = 0; j < 0x3600; j++); // Delay for 1.2V ref startup

SD24CCTL1 |= SD24SC; // Set bit to start conversion |


}

void gain_adjust()
{
//P1.7 Gain_2, P1.6 Gain_1

// Gain_2 | Gain_1 | R | | Ganho R1 = 470
// 0 0 470 R 2.6 R2 = 150
// 0 1 235 (R//R1) 4.2
// 1 0 113 (R//R2) 6.0
// 1 1 110 (R//R1//R2) 7.6

unsigned short int c = 0;
// P2DIR |= BIT0; //LED
// P2OUT &= ~BIT0; //LED
P1IE |= BIT4; // P1.4 interrupt enabled
P1IES |= BIT4; // P1.4 Hi/lo edge
P1IFG &= ~BIT4; // P1.4 IFG cleared
P1DIR |= BIT7 | BIT6;
// P1OUT &= ~BIT7 & ~BIT6;
gain_state = gain_1;
while (c!=1)
{
// Machine state to gain adjust
switch(gain_state)
{
case gain_1:
P1OUT &= ~BIT7 & ~BIT6;
__delay_cycles(20320000); // Delay
if (Port_flag == 1) //Verify if port stay high
{
gain_state = gain_2;
}
else //Minimum gain doesnt work in this powerline
{
c = 1;
}
break;
case gain_2:
P1OUT |= BIT6;
__delay_cycles(20320000); // Delay
if (Port_flag == 1)
{
// P1OUT = BIT6; //Set P1.6 to increase gain (4.2)
gain_state = gain_3;
}
else
{
gain_state = gain_1;
P1OUT &= ~BIT6;
c=1; //Minimum gain doesnt work in this powerline
}
break;

case gain_3:
P1OUT &= ~BIT6;
P1OUT |= BIT7;
__delay_cycles(20320000); // Delay
if (Port_flag == 1)
{
// P1OUT = BIT7; //gain2 is ok. Lets increase this gain (6.0)
gain_state = gain_4;
}
else
{
P1OUT &= ~BIT7;
P1OUT |= BIT6;
gain_state = gain_2;
c=1;
// P1OUT &= ~BIT6; //gain2 is too high, lets return to minimum gain
}
break;

case gain_4:
P1OUT |= BIT6;
__delay_cycles(20320000); // Delay
if (Port_flag == 1)
{
// P1OUT |= BIT6; //Set P1.6 to increase gain (7.6)
// gain_state = gain_end;
c=1;
}
else
{
P1OUT &= ~BIT6;
gain_state = gain_3;
// P1OUT = BIT6; //gain3 is too high, lets return to gain2
c=1;
}
break;
default:
gain_state = gain_1;
}
}
P1IE &= ~BIT4; // P1.4 interrupt enabled

}

//start,MeterId,action,end
void command(unsigned char c)
{
if(c == '#')
{
// P2OUT ^= BIT0;
uart_state = ready;
}

else
{
if(uart_state != iddle)
{
switch(uart_state)
{
case ready:
if(c == '3')
{
uart_state = id;
}
else uart_state = iddle;
break;

case id:
switch(c)
{
case 'g':
uart_state = get;
break;
case 's':
uart_state = set;
break;
case 'r':
uart_state = reset;
break;
default:
uart_state = iddle;
}
break;

case get:
if(c == ';')
{
send = 1;
}

uart_state = iddle;
break;

case set:
if(c == ';')
{
send_relay = 'L';
}

uart_state = iddle;
break;

case reset:
if(c == ';')
{
send_relay = 'D';
}
uart_state = iddle;
break;

default:
uart_state = iddle;
}
}
}
}

void send_param(f)
{
unsigned int count = 0;
unsigned int send_count;

IE1 = 0x00; // Disable USART0 RX interrupt

U0TXBUF = '*'; // Send Header
while((U0TCTL & TXEPT) != 1);

// Only for Labview //
// //Send Voltage Wave
// for(count = 0; count < SAMPLE_CYCLE; count ++)
// {
// voltage_wave.all_wave = V_buffer[count];
// for(send_count = 2; send_count > 0; send_count --)
// {
// U0TXBUF = voltage_wave.pt_wave[(send_count-1)];
// while((U0TCTL & TXEPT) != 1);
// }
// }

// count = 0;
// // Send Current Wave
// for(count = 0; count < SAMPLE_CYCLE; count ++)
// {
// current_wave.all_wave = I_buffer[count];
// for(send_count = 2; send_count > 0; send_count --)
// {
// U0TXBUF = current_wave.pt_wave[(send_count-1)];
// while((U0TCTL & TXEPT) != 1);
// }
//
// }
//------------------------------------------------------------------------//
//Send Voltage RMS
for(count=4;count>0;count--) // Loop to send the voltage float value
{
U0TXBUF = voltage.pt_VI[(count-1)];
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
}
//Send Current RMS
for(count=4;count>0;count--) // Loop to send the current float value
{
U0TXBUF = current.pt_VI[(count-1)];
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
}
//Send PowerFactor
for(count=4;count>0;count--) // Loop to send the current float value
{
U0TXBUF = PowerFactor.pt_VI[(count-1)];
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
}
//Send Active Energy
for(count=4;count>0;count--) // Loop to send the current float value
{
U0TXBUF = energy.pt_VI[(count-1)];
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
}
//Send Reactive Energy
for(count=4;count>0;count--) // Loop to send the current float value
{
U0TXBUF = ReactEnergy.pt_VI[(count-1)];
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
}
//Send ActPower
for(count=4;count>0;count--) // Loop to send the current float value
{
U0TXBUF = ActPower.pt_VI[(count-1)];
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
}
//Send ReactPower
for(count=4;count>0;count--) // Loop to send the current float value
{
U0TXBUF = ReactPower.pt_VI[(count-1)];
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
}

////-------- Labview--- //
// U0TXBUF = f; //Send END
// while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete
//// ---------------- //
U0TXBUF = '!'; //Send END
while((U0TCTL & TXEPT) != 1); // Wait for the flag TXEPT -> Transmission Complete

IE1 = URXIE0; // Enaable USART0 RX interrupt

}

void relay(unsigned char command)
{
switch(command)
{
case 'L':
P1OUT |= BIT0; //Turn on relay

// IE1 = 0x00; // Disable USART0 RX interrupt
// U0TXBUF = '*'; // Send Header
// while((U0TCTL & TXEPT) != 1);
//
// U0TXBUF = '1'; // Send Id
// while((U0TCTL & TXEPT) != 1);
//
// U0TXBUF = 'i'; // Send Turnoff
// while((U0TCTL & TXEPT) != 1);
//
// U0TXBUF = '!'; // Send End
// while((U0TCTL & TXEPT) != 1);
// IE1 = URXIE0; // Enaable USART0 RX interrupt

send_relay = 'N';
break;

case 'D':

P1OUT &= ~BIT0; //Turn on relay
// IE1 = 0x00; // Disable USART0 RX interrupt
// U0TXBUF = '*'; // Send Header
// while((U0TCTL & TXEPT) != 1);
//
// U0TXBUF = '1'; // Send Id
// while((U0TCTL & TXEPT) != 1);
//
// U0TXBUF = 'o'; // Send Turnoff
// while((U0TCTL & TXEPT) != 1);
//
// U0TXBUF = '!'; // Send End
// while((U0TCTL & TXEPT) != 1);
// IE1 = URXIE0; // Enaable USART0 RX interrupt
send_relay = 'N';
break;
default:
send_relay = 'N';
}
}

void calculate()
{
unsigned int count;

V1_avg = V_buffer_accum / SAMPLE_CYCLE; //Average value
I1_avg = I_buffer_accum / SAMPLE_CYCLE; //Average value

for(count=0;count<SAMPLE_CYCLE;count++) //Subtract average value for each sample
{
V_buffer[count] -= V1_avg;
I_buffer[count] -= I1_avg;

}
for(count=0;count<SAMPLE_CYCLE;count++) //Loop for RMS Calculations
{
I_operand = I_buffer[count];
V_operand = V_buffer[count];
I_acum += I_operand * I_operand;
V_acum += V_operand * V_operand;
P_acum += V_operand * I_operand;
}

argument = I_acum / SAMPLE_CYCLE; //RMS Calculation
I_rms = sqrt(argument);
argument = 0;

argument = V_acum / SAMPLE_CYCLE; //RMS Calculation
V_rms = sqrt(argument);
argument = 0;

argument=(P_acum/SAMPLE_CYCLE); //Calculating the Active Power value
P = argument * ka * kv;
if (P < 0)
{
P=0;
}
argument=0;

voltage.all_VI = V_rms * kv; //Adjust real voltage value
current.all_VI = I_rms * ka; //Adjust real current value
ActPower.all_VI = P;

S=voltage.all_VI*current.all_VI; //Calculating Apparent Power
ReactPower.all_VI = S;
PF=P/S; //Calculating the Power Factor
PowerFactor.all_VI = PF;

E += P * kw; //Calculating energy in Wh
energy.all_VI = E;
React_E += S * kw;
ReactEnergy.all_VI = React_E;

s_count=0; //clear sample count
I_acum=0; //clear accumulators
V_acum=0;
P_acum=0;
I_buffer_accum = 0;
V_buffer_accum = 0;
V1_avg = 0; //clear average values
I1_avg = 0;

}


void PWM(idx, s)
{
if (s == 1) //PWM ON
{
TACCTL1 = 0x00; //Clear PWM configuration
R0 = LimR0[idx]; //frequency vector
R1 = LimR1[idx]; // duty cycle vector
// R0 = 42; //frequency vector
// R1 = 21; // duty cycle vector
TACTL = 0x00;
TACTL |= TACLR; //Clear Timer A Counter
TACCR0 = R0; // PWM Frequency
TACCTL1 = OUTMOD_6; // CCR1 toggle/set
TACCR1 = R1; // PWM duty cycle
TACTL = TASSEL_2 + MC_1; // SMCLK, up mode
}
else //PWM OFF
{
TACCTL1 = 0x00;
}

}

int PWM_adjust()
{
unsigned short int i,j=0,f=0;
short int k_counter = 0;
short int s[23] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
// short int k[23] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
freq_adjust_flag = 1;

// Sweep frequency routine
/* each 'i' value is related to frequency vector position in PWM function, so
* PWM functions will run 23x to sweep all frequencies sending a T character test.
* In the beginning If the system receive a T character successfully, k[i] = 1 and s[i] (1)
* At the end, an average of the interval which the T character was successfully received is made
*/

for(i=0; i<FREQUENCY_AMOUNT; i++)
{
PWM(i,1);
__delay_cycles(100);
U0TXBUF = TEST;
while((U0TCTL & TXEPT) != 1);
__delay_cycles(100);

if (bufferRX == TEST)
{
// P2OUT = BIT0;
// k[i] = 1;
s[i] = i;
k_counter += 1;
}
else
{
// k[i] = 0;
s[i] = 0;
}

j += s[i];
// _delay_cycles(108550000);
}
if (k_counter == 0)
{
f = 0;
}
else
{
f = j / k_counter;
}
freq_adjust_flag = 0;
return f;
}

void configura_timer(short int s)
{
if (s == 1)
{
CCTL0 = CCIE; // CCR0 interrupt enabled
CCR0 = 54997; //~20ms
TACTL = TASSEL_2 + MC_1 + ID_3; // SMCLK, upmode, SMCLK/8
}
else
{
TACTL = TACLR;
}

}

#pragma vector=USART0RX_VECTOR
__interrupt void USART0RX ()
{
if (freq_adjust_flag == 1) // a way to separate the frequency sweep and the command of the system
{
bufferRX = U0RXBUF;
}
else
{
// P2OUT ^= BIT0;
command(U0RXBUF);
}


}

#pragma vector=SD24_VECTOR
__interrupt void SD24AISR(void)
{
switch (SD24IV)
{
case 2: // SD24MEM Overflow
break;
case 4: // SD24MEM0 IFG
V_AD_RESULT = SD24MEM0;
I_AD_RESULT = SD24MEM1;
V_buffer[s_count] = V_AD_RESULT;
I_buffer[s_count] = I_AD_RESULT;
V_buffer_accum += V_AD_RESULT; // Accum to calculate average
I_buffer_accum += I_AD_RESULT;
s_count++;
break;
case 6: // SD24MEM1 IFG
break;
case 8: // SD24MEM2 IFG
break;
}

}

#pragma vector=PORT1_VECTOR
__interrupt void Port_1(void)
{
//If this interrupt occurs, then some gain is turning P1.4 off
// P2OUT = BIT0;
Port_flag = 0;
P1IFG &= ~BIT4; // P1.4 IFG cleared
}

#pragma vector=TIMERA0_VECTOR
__interrupt void Timer_A (void){
CCR0 = 54997;
}


void main(void)
{
clock_init();
__bis_SR_register(GIE); // Enable interrupt
gain_adjust();
port_init();
configura_timer(1);
calcula_baudrate();
configura_timer(0);
UART_init();
frequency = PWM_adjust();
PWM(frequency,1);
sd_init();


while(1)
{
if(s_count == SAMPLE_CYCLE) // S_COUNT = SAMPLE_CYCLE
{
P2OUT ^= BIT0;
SD24CCTL1 &= ~SD24SC; // Set bit to stop conversion
calculate();
// test
// PWM(frequency,1);
// U0TXBUF = 'T';
// while((U0TCTL & TXEPT) != 1);
// PWM(frequency,0);
if(send == 1)
{
P2OUT ^= BIT0;
PWM(frequency,1);
send_param(frequency);
PWM(frequency,0);
send = 0;
}
if(send_relay != 'N')
{
// PWM(frequency,1);
relay(send_relay);
// PWM(frequency,0);
}
// SD24CCTL1 |= SD24SC;

}
}

}

**Attention** This is a public forum