Hi,
we are having issue of "Region ROM Overflow" with MSP430F5419A.
Our actual code size is less than 42K, and MSP430F5419A supports up to 128K memory.
we are using GCC compiler4.6.3.
Kindly advise.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
we are having issue of "Region ROM Overflow" with MSP430F5419A.
Our actual code size is less than 42K, and MSP430F5419A supports up to 128K memory.
we are using GCC compiler4.6.3.
Kindly advise.
Hi,
I have checked the ldscript file and the sections are not overlapping.
Please check following file for more details. Here my code size is crossing the limit of 41K of rom size and that is why the overlapping message was displayed.
MEMORY {
sfr : ORIGIN = 0x0000, LENGTH = 0x0010 /* END=0x0010, size 16 */
peripheral_8bit : ORIGIN = 0x0010, LENGTH = 0x00f0 /* END=0x0100, size 240 */
peripheral_16bit : ORIGIN = 0x0100, LENGTH = 0x0100 /* END=0x0200, size 256 */
bsl : ORIGIN = 0x1000, LENGTH = 0x0800 /* END=0x1800, size 2K as 4 512-byte segments */
infomem : ORIGIN = 0x1800, LENGTH = 0x0200 /* END=0x1a00, size 512 as 4 128-byte segments */
infod : ORIGIN = 0x1800, LENGTH = 0x0080 /* END=0x1880, size 128 */
infoc : ORIGIN = 0x1880, LENGTH = 0x0080 /* END=0x1900, size 128 */
infob : ORIGIN = 0x1900, LENGTH = 0x0080 /* END=0x1980, size 128 */
infoa : ORIGIN = 0x1980, LENGTH = 0x0080 /* END=0x1a00, size 128 */
ram (wx) : ORIGIN = 0x1c00, LENGTH = 0x4000 /* END=0x5c00, size 16K */
rom (rx) : ORIGIN = 0x5c00, LENGTH = 0xa380 /* END=0xff80, size 41852 */
vectors : ORIGIN = 0xff80, LENGTH = 0x0080 /* END=0x10000, size 128 as 64 2-byte segments */
far_rom : ORIGIN = 0x00010000, LENGTH = 0x00035c00 /* END=0x00045c00, size 215K */
/* Remaining banks are absent */
ram2 (wx) : ORIGIN = 0x0000, LENGTH = 0x0000
ram_mirror (wx) : ORIGIN = 0x0000, LENGTH = 0x0000
usbram (wx) : ORIGIN = 0x0000, LENGTH = 0x0000
}
REGION_ALIAS("REGION_TEXT", rom);
REGION_ALIAS("REGION_DATA", ram);
REGION_ALIAS("REGION_FAR_ROM", far_rom);
PROVIDE (__info_segment_size = 0x80);
PROVIDE (__infod = 0x1800);
PROVIDE (__infoc = 0x1880);
PROVIDE (__infob = 0x1900);
PROVIDE (__infoa = 0x1980);
The portion marked in yellow colour indicates start location and using length we can calculate end location.
It’s not overlapping.
Kindly advise.
**Attention** This is a public forum