This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5528: Operating Temperature Range

Part Number: MSP430F5528

Hello,

Looking at the datasheet, both the recommended operating free-air temperature and operating junction temperature ranges are listed as -40 to +85C. If the ambient temperature is +85C and the device is dissipating any power, the junction temperature spec will be violated... so it seems incorrect that both maximum temperatures can be +85C.

I'm hoping that the datasheet is incorrect, and that someone could identify what the correct maximum junction temperature for this device (specifically, PN MSP430F5528IYFF) is.

Regards,

Jason

**Attention** This is a public forum