This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5969: LPM4

Part Number: MSP430FR5969

Tool/software: Code Composer Studio

hi this is harikrishna....

currently i am working on the low power modes..for better current consumption i am using LPM4 in my project..and i refer the MSP430FR5969 user guide and data sheeet..it says that in LPM4 only external interrupt will only wake_up from the low_power_mode...but in my project  i am using external 32768HZ(ACLK=32K) crystal and RTC is Still running with that 32K..how it is possible..or  RTC will run in  LPM4 mode...or my MSP is not working properly..really i don't no what is happen..can anybody tell me the problem..

**Attention** This is a public forum