This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F233: MSP430F233 External oscillator with SMCLK at 16Mhz

Part Number: MSP430F233


Tool/software: Code Composer Studio

Hi,

I'm trying to configure my UART to use a SMCLK with a frequency of 16 MHz, and also using an external oscillator (XT2CLK).  I've tried configuring the baud rate and modulation from the User's Guide and reading the Basic Clock Module chapter in the User's Guide as well.  Every time I test the UART comm pin on my MCU, I don't seem to be getting a consistent stream of serial data. I've added my UART config code below. Am I overlooking an extra calibration control register or do need to get rid of any registers in my code?

 UART Initialization

P3SEL = 0x30; // P3.4,5 = USCI_A0 TXD/RXD

BCSCTL2 = SELM_2 | DIVM_0 | SELS | DIVS_1;

DCOCTL = 0x00;

BCSCTL1 |= DIVA_0;

BCSCTL1 &= ~XT2OFF;

BCSCTL3 = XT2S_3 | LFXT1S_0 | XCAP_0;

CCTL0 = CCIE; // CCR0 interrupt enabled

CCR0 = 40000;

TACTL = TASSEL_2 + MC_2; // SMCLK, contmode

UCA0CTL1 |= UCSWRST; // **Put state machine in reset**

UCA0CTL1 |= UCSSEL_2; // Clock Source SMCLK

UCA0BR0 = 138; // 16MHz 115200

UCA0BR1 = 0; // 16MHz 115200

UCA0MCTL = UCBRS_7 + UCBRF_0; // Modulation UCBRSx = 7

UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**

IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt


Thanks

**Attention** This is a public forum