This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2533: Datasheet error

Part Number: MSP430G2533


Kindly confirm on datasheet error below.

We discovered that the documentation for the TI MSP430G2533 (28-pin package) is not correct. Specifically, two of the timer pins are mislabelled:

Pin 10: TA1.0 is actually TA1.1

Pin 11: TA1.1 is actually TA0.1

 

Mixing channel 1 & 2 on a timer is not generally a major problem, but in both of the cases above it involved channel 0, which has limitations when it comes to certain functions, such as PWM. We are using these pins for PWM and had to be certain and spent a bunch of time verifying these discrepancies. There may be other mis-documented pins but we limited the scope of our testing.

 

Anyway, this is just an FYI, and perhaps TI could update their documentation.

 

http://www.ti.com/lit/ds/symlink/msp430g2533.pdf

**Attention** This is a public forum