This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2632: Loaded image does not work after being programmed via spy-bi-wire

Part Number: MSP430FR2632

I am able to flash the hex file generated from CCS onto my board via Spy-bi-wire. I am also able to read out the memory address spaces to verify that the correct values are loaded onto the various memory address locations. However, the loaded image doesn't seem to be running despite us having done V_RESET. Should i be doing something else to get the program to start running?

**Attention** This is a public forum