Part Number: MSP430F6734A
Hi,
A few days ago I was playing with the security options of MSP430F6734A in IAR.
I have added below pragma code in IAR, and Project Options->Debugger->FET Debugger->Download->"Allow erase/write access to BSL Flash Memory" and programmed the MSP properly.
After that program, I commented pragma code below and continue developing my application without any restriction. During that time I reprogram MSP430 maybe 10 times and never faced an issue.
#pragma location = 0x17FC
__root const uint8_t JTAG_password[] = {0x11, 0x22, 0x33, 0x44}; // -> 0x22114433
Today, I guess first time of power cycle of the device (power off and on), JTAG interface started giving following error:
"The Debug Interface to the device has been secured"
The part that we use MSP430F6734A, it has Device Descriptors in range 1A00h - 1AFFh that contain some ADC calibration parameters.
I don't want to erase BSL or Device Descriptors sections of the device.
I know the jtag password but still can't access. JTAG password editbox in IAR options is disabled, I don't know why.
I have tried MSP430Flasher like below but no chance:
MSP430Flasher.exe -w "USB_PRE.txt" -p 0x22114433 -v -g -z [VCC]
# Exit: 16
# ERROR: The Debug Interface to the device has been secured
How can I bring it back to unsecured position without losing BSL or Device Descriptor sections?
Thanks.