Part Number: CC430F5137
Other Parts Discussed in Thread: TPS560200, TPS62172, SIMPLICITI,
I am developing a project based on cc430f5137. This is a wireless network based on Simpliciti. The power supply of the microcontroller cc430f5137 is made from a pulse step-down converter TPS560200. However, some (not all) microcontrollers start to heat up very much and consume more than 300 mA. Activities that I have already done: 1. All "hanging in the air" outputs of the microcontroller tuned to the input with a pull-up to power. 2. I changed the converter (used to be TPS62172), everyone used to heat up, now some. 3. All the settings made by errata SLAZ094X. I measured the oscilloscope output TPS560200, nothing special. I can not understand what's the matter!