Part Number: CC430F5123
Tool/software: TI-RTOS
thaks,
do you mean that the typical application circuit cc430f51xx on figure 30 in "msp430 soc with rf core" can be used for my design
which receive rf 447mhz signal from rf 447mhz transmitter.
and the bill of materials(for 433mhz) on table 49 on page 85 of "msp430 soc with rf core" will be ok for rf447mhz .
and what about rf antena. do i use regular 5o ohm antena?
my design is two separate system. one is transmitter which transmit signal with domestic product with 447mhz band that have license in our country
and second i have to design a receiver with 447mhz band which do not need license with ti's cc430f5123 module.
the function is very simple. transmitter will send signal under 100byte and the receiver will receive above data only wirelessly about 200 meters apart.
anyway pls acknowlege me any other cheap and useful item what i intend.
regards,