Other Parts Discussed in Thread: MSP-EXP430FR5994
Hi Team 430,
The MSP-EXP430FR5994 EVM used to ship w/ an included uSD card in the box.. but is no longer included Which class of uSD card used to ship w/ the EVM? I do not see this mentioned in the Users Guide (slau678) or Quick Start Guide (slau677).. I recommend that it be added.
It seems there was a non-trivial change in the SD Card Spec between Class6 and Class10 WRT the SD Card SPI specs. Which Class(es) of SD card will work properly w/ the sample software provided w/ the EVM?
Thanks, Merril