Hello,
I am a beginner and I am looking for a Development board which has on board Micro-controller, Memory, High speed ADC (20MSPS) etc. In my searching I am not able to find such a board in the TI Development kits. Please correct me if i am wrong. In my application I mounted a PVDF sensor on a cylindrical rod and rod is rotated by 10° with stepper motor and i want to read the sensor value at every 10°. I got an analog output signal from my sensor in mV with 5.5 MHz frequency. I want to read and store that output as a Raw data in PC. Currently I am using Arduino but it is not capable enough for recording my signal. I also had a MSP430 Launchpad but it is also not an ideal for that So I have to switch for some alternatives. For that, Is there any single board which has on board high sampling rate ADC (~20 MSPS) can fulfill my all requirement ?
or You can suggest me how to achieve it. I welcome you for your valuable suggestions and feedback. Thanking you!
Best Regards,