Part Number: MSP430F6736
Tool/software: Code Composer Studio
Hi Team,
I want to generate a .CSV file using the outputs that I print on the console(in CSV format).
I want to export the values that I print on the console to a .CSV file.
I am using the following code:
#include <msp430.h>
#include <stdio.h>
#include <time.h>
/* Array to store SD24_B conversion results */
unsigned int results[3]; //SD24 converter result array
unsigned int ADC_Result[6]; // 8-bit ADC conversion result array
float A0,A1,A2,A3,A4,A5,A6,A7,A8; //analog voltage result registers
float I0,I1,I2,I3,I4,I5,I6,I7,I8; //current result registers
unsigned int sig=0x0;
time_t current_time;
char *c_time_string;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// Setup P1.2 A0, 1.1 A1, 1.0 A2
P1SEL |= BIT0 | BIT1 | BIT2; // Set P1.0,.1,.2 to non-IO
P9SEL |= BIT1 | BIT2 | BIT3; //set P9.1,.2,.3 to non-IO
P5DIR |= BIT0 | BIT1 | BIT2 | BIT3;
__disable_interrupt(); // Disable interrupts; Port Map cnfg
PMAPKEYID = PMAPKEY; // Enable access Port Mapping regs
P1MAP2 = PM_ANALOG; // Enable A0
P1MAP1 = PM_ANALOG; // Enable A1
P1MAP0 = PM_ANALOG; // Enable A2
PMAPKEYID = 0; // Disable access Port Mapping regs
__enable_interrupt(); // Re-enable all interrupts
// Setup ADC10
ADC10CTL0 = ADC10SHT_3 | ADC10MSC | ADC10ON; // 16 ADCclks, MSC, ADC ON
ADC10CTL1 = ADC10SHP | ADC10CONSEQ_1; // pulse sample mode, single sequence
ADC10CTL2 |= ADC10RES; // 8-bit resolution
ADC10MCTL0 = ADC10INCH_5; // A0,A1,A2(EoS), AVCC reference
// Setup DMA0 (ADC10IFG trigger)
DMACTL0 = DMA0TSEL_24; // ADC10IFG trigger
DMA0SZ = 0x06; // 3 conversions
__data16_write_addr((unsigned short) &DMA0SA, (unsigned long) & ADC10MEM0);
// Source single address
__data16_write_addr((unsigned short) &DMA0DA, (unsigned long) & ADC_Result[0]);
// Destination array address
DMA0CTL = DMADT_4 | DMADSTINCR_3 | DMAEN | DMAIE;
DMA0CTL &= ~DMASRCBYTE;
DMA0CTL &= ~DMADSTBYTE;
// Repeated single transfer
// Increment destination
// Byte access
// Enable int after seq of convs
SD24BCTL0 |= SD24SSEL_1; // Select internal REF
SD24BCTL0 &= ~SD24REFS; // Select SMCLK as SD24_B clock source
SD24BCCTL0 &= ~SD24SNGL;
//SD24BCCTL0 |= SD24ALGN;
SD24BCCTL0 |= SD24DF0;
SD24BCCTL0 |= SD24SCS_5; // Single conversion, group 1
SD24BCCTL1 &= ~SD24SNGL;
//SD24BCCTL1 |= SD24ALGN;
SD24BCCTL1 |= SD24DF0;
SD24BCCTL1 |= SD24SCS_5; // Single conversion, group 1
SD24BCCTL2 &= ~SD24SNGL;
//SD24BCCTL2 |= SD24ALGN;
SD24BCCTL2 |= SD24DF0;
SD24BCCTL2 |= SD24SCS_5; // Single conversion, group 1
SD24BIE |= SD24IE2; //| SD24IE1 | SD24IE0; // Enable channel 2 interrupt
printf("\" \",\"V1\",\"Supply\",\"V2\",\"Supply\",\"Time\"\n");
printf("\" \",\"voltage(in V)\",\"current(in A)\",\"voltage(in V)\",\"current(in A)\"\n");
__delay_cycles(0x10000); // Delay for 1.5V REF startup
while (1)
{
//time setup
time_t t = time(NULL);
struct tm *tm = localtime(&t);
char s[64];
strftime(s, sizeof(s), "%c", tm);
while (ADC10CTL1 & ADC10BUSY) ; // Wait if ADC10 core is active
ADC10CTL0 |= ADC10ENC | ADC10SC; // Sampling and conversion start
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0 w/ interrupts
__delay_cycles(1000); // Delay between sequence convs
__no_operation(); // BREAKPOINT; View ADC_Result
//ADC_10 voltage and current display
A0=(ADC_Result[5]*3.3)/(1024*5);
I0=(A0)/2.43;
A1=(ADC_Result[4]*3.3)/(1024*5);
I1=(A1)/2.43;
A2=(ADC_Result[3]*3.3)/(1024*5);
I2=(A2)/2.43;
A3=(ADC_Result[2]*3.3)/(1024*5);
I3=(A3)/2.43;
A4=(ADC_Result[1]*3.3)/(1024*5);
I4=(A4)/2.43;
A5=(ADC_Result[0]*3.3)/(1024*5);
I5=(A5)/2.43;
printf("\"A5\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A5,I5,s);
//printf(" %s current I5= %f \n",s,I5);
printf("\"A4\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A4,I4,s);
//printf("\n %s analog voltage A4= %f \n",s,A4);
//printf(" %s current I4= %f \n",s,I4);
printf("\"A3\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A3,I3,s);
//printf("\n %s analog voltage A3= %f \n",s,A3);
//printf(" %s current I3= %f \n",s,I3);
printf("\"A2\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A2,I2,s);
//printf("\n %s analog voltage A2= %f \n",s,A2);
//printf(" %s current I2= %f \n",s,I2);
printf("\"A1\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A1,I1,s);
//printf("\n %s analog voltage A1= %f \n",s,A1);
//printf(" %s current I1= %f \n",s,I1);
printf("\"A0\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A0,I0,s);
//printf("\n %s analog voltage A0= %f \n",s,A0);
//printf(" %s current I0= %f \n",s,I0);
SD24BCTL1 |= SD24GRP1SC; // Set bit to start conversion
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0 w/ interrupts
SD24BCTL1 &= ~SD24GRP1SC; // Clear bit for next conversion
__no_operation(); // SET BREAKPOINT HERE
//SD24 converter voltage and current display
A6=(results[0]*3.3)/(256*5);
I6=(A6)/2.43;
A7=(results[1]*3.3)/(5*256);
I7=(A7)/2.43;
A8=(results[2]*3.3)/(256*5);
I8=(A8)/2.43;
printf("\"A6\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A6,I6,s);
//printf("\n %s analog voltage A6= %f \n",s,A6);
//printf(" %s current I6= %f \n",s,I6);
printf("\"A7\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A7,I7,s);
//printf("\n %s analog voltage A7= %f \n",s,A7);
//printf(" %s current I7= %f \n",s,I7);
printf("\"A8\",\"%f\",\"%f\",\" \",\" \",\"%s\"\n",A8,I8,s);
//printf("\n %s analog voltage A8= %f \n",s,A8);
//printf(" %s current I8= %f \n",s,I8);
__delay_cycles(2000);
if (sig==0x10)
{
sig = 0x00;
}
else
{
printf("select line chosen= %d \n",sig);
P5OUT = sig;
sig++;
}
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=SD24B_VECTOR
__interrupt void SD24BISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(SD24B_VECTOR))) SD24BISR (void)
#else
#error Compiler not supported!
#endif
{
switch (SD24BIV)
{
case SD24BIV_SD24OVIFG: // SD24MEM Overflow
break;
case SD24BIV_SD24TRGIFG: // SD24 Trigger IFG
break;
case SD24BIV_SD24IFG0: // SD24MEM0 IFG
break;
case SD24BIV_SD24IFG1: // SD24MEM1 IFG
break;
case SD24BIV_SD24IFG2: // SD24MEM2 IFG
results[0] = SD24BMEMH0; // Save CH0 results (clears IFG)
results[1] = SD24BMEMH1; // Save CH1 results (clears IFG)
results[2] = SD24BMEMH2; // Save CH2 results (clears IFG)
break;
}
__bic_SR_register_on_exit(LPM0_bits); // Exit LPM0
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=DMA_VECTOR
__interrupt void DMA0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(DMA_VECTOR))) DMA0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch (__even_in_range(DMAIV, 16))
{
case DMAIV_NONE: break; // No interrupts
case DMAIV_DMA0IFG: // DMA0IFG = DMA Channel 0
// sequence of conversions complete
__bic_SR_register_on_exit(LPM0_bits); // exit LPM0 on return
break;
case DMAIV_DMA1IFG: break; // DMA1IFG = DMA Channel 1
case DMAIV_DMA2IFG: break; // DMA2IFG = DMA Channel 2
case 8: break; // Reserved
case 10: break; // Reserved
case 12: break; // Reserved
case 14: break; // Reserved
case 16: break; // Reserved
default: break;
}
}
Is there a way to generate a .CSV file?
Thank you,
Keval