Part Number: MSP430F5418A
MSP430F5418A is used in an ACCL (Auto source changeover and current limit) card. MSP430F5418A is driven by two powersupply one from EB (Electricity board) and another through DG (Diesel Generator). Schematic attached.
Issues:
- During changeover from EB to DG or DG to EB power source, microcontroller is getting reset once is five times of the changeover. Please note that customer is deriving power from both EB and DG to power up microcontroller.
- Customer is using 32.76Khz external crystal. Earlier when 20Mhz crystal was used frequency of resetting was more. Can MSP430F5418A be used with 20MHz crystal for auto source change over application?
- Customer is using 74HC573 to drive the LEDs as seen in schematic attached. Customer wanted to know if it is possible for MSP430F5418A to drive LEDs directly without using 74HC573?
- Microcontroller is displaying Ir, Ib, Iy (load currents) though no load is connected in the circuit.
Please let us know possible debug steps to resolve the above issues.SCH_PDENACCL_R3.pdf