Other Parts Discussed in Thread: MSP-TS430RHB32A
Tool/software: TI C/C++ Compiler
Test condition:
- MSP-TS430RHB32A board
- GAIN 1
- Measuring result = 10 data average
- sample program "sd24_ex4_singleConversionSingleChannelPolling"
- supply volt.: 3.3V (Tenma 72-10480 DC Power supply)
I have test the 24-Bit ADC function and capture the data.
However, I find got many noise even I short the pin of A0 and A1. (the result is attached)
the max volt = 0.00017767 V, the min. volt. = 0.000158358
diff. volt. = 19.3 uV
Best regards,
Mr. Hung