Part Number: MSP430AFE253
Other Parts Discussed in Thread: MSP430I2041, TIDM-3OUTSMTSTRP, , MSP-EM-DESIGN-CENTER
Hi,
I'm trying to create a simple energy meter that have also the option to switch on/off the load power using 2 relays.
The energy meter works just fine as long as I do not switch on the relays with a load on. Once I'm issuing the command to turn the relays ON, the microcontroller gets fried.
I have tried also with a current transformer, but the results are the same, except that the microcontroller gets fried after 3-4 ON commands.
The shunt resistor is very close the relay that switches the N line, but the N line is switched ON first and than the L line is switched ON after the zero crossing is detected.
I'm attaching an image with the analog front end.
The power supply that supplies the voltages for the design is an AC/DC non-isolated converter.
Is there a way to isolate the damaging effect that the relays induce once they are switched ON?
Best regards,
Cristian