This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5342: Problem debug custom BSL

Part Number: MSP430F5342
Other Parts Discussed in Thread: MSP430-FLASHER

Tool/software: Code Composer Studio

Hello
I'm trying to write a custom BSL from the examples provided by TI, using the CCS8 environment.  I managed to compile a small example (turning on an LED) and I verified that the program was actually compiled to be stored in the BSL area.

When I try to load it with the emulator, I receive the following error:

MSP430: File Loader: Verification failed: Internal error while writing 0x01010

In practice, I understand that I can not access the BSL area in writing.

Yet in the project properties -> debugging -> MSP430 Flash Setting I set:

Allow read / write / erase access to BSL memory

and

Erase main, information and protected information memory

Where am I wrong?

Thank you

**Attention** This is a public forum