This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6989: What is the maximum number of GPIO in this MCU

Part Number: MSP430FR6989
Other Parts Discussed in Thread: ENERGIA, , MSP-EXP430FR6989, MSP-TS430PZ100D, MSP430FR5994, MSP432E401Y

Hi,

I am using MSPFR6989 to output 18 signals to the GPIO (through using writeAnalog function in Energia) and read 9 signals through the ADC, the issue I'm facing is I found only 16 pins available , I tried to use extra pins of p1.0 and p9.7, for p1.0 it receives the right voltage when I checked by the voltmeter but p9.7 is not, how can I solve this issue? 

Thank you

**Attention** This is a public forum