This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P4111: My board is about 55 degrees celsius

Part Number: MSP432P4111


I was using the MSP432P411, and a few moments later the board temperaure increased about +25º the normal temperature is 25º and now is 55º

What should I do?

When I debbug with CCS this error appear

CORTEX_M4_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)


CORTEX_M4_0: JTAG Communication Error: (Error -615 @ 0x0) The target failed to see a correctly formatted SWD header. The connection to the target may be unreliable. Try lowering the TCLK setting before trying again. (Emulation package 8.0.27.9)

**Attention** This is a public forum