Gents - We have two of these boards; just acquired a couple of days ago in order to assess this platform...
One of these works perfectly out of the box; connects to Exosite, added to a product. All good.
The second I cannot get to connect - am using same switch port to same world-facing IP address. At first was getting a 502 (Gateway?) Error. Have soft reset the card several times...
Have also re-built the OOB example from scratch and reinstalled.
Have even added Rei Vilo's suggestion to the code, thinking this would help the reset. No luck! :
In order to wipe the old PID from EEPROM, just add EraseEEPROM() after NVSInit() in main_tirtos.c
The screen command (even after killing its process) displays nothing:
$ screen /dev/cu.usbmodemME401021 115200 –L