Part Number: MSP430F6725A
Other Parts Discussed in Thread: MSP430F6723, MSP430F6723A, , UNIFLASH, MSP430F6730, MSP-FET
Tool/software: Code Composer Studio
When installing the MK (MSP430F6725A IPN (TI) on the device card in replaceable MSP430F6723A IPN (TI) and MSP430F6723 IPN (TI), it turned out that they do not work, although the documentation says that they are interchangeable.
The fact is that we connect to the controller via MSP-EXP430G2 (LaunchPad), as well as to all the others.
But MSP430F6725A is not defined at all, so it's impossible to load the code into the MK.
Also it is impossible to determine the controller through UniFlash v4.
The voltage is normal, there are several devices, all are not working, two other types of MK, for example such as (MSP430F6723, MSP430F6730) work on this board, because they are also interchangeable.
After the MSP430F6725A is soldered to the same card, it stops appearing.