Part Number: MSP430F5342
Other Parts Discussed in Thread: MSP430F5340
Hi,
I have following requirements
Memory > 48 KB (max), RAM > 4 KB (Max), UART -2 , SPI -4, GPIO with Interrupts - 8
Also I need BSL programming via UART.
Also the package can be LQFP/VQFN/TSSOP with size less than 10mmx10mm.
I have shortlisted MSP430F5342 as a possible candidate.
Can anybody suggest a better controller having the above features and providing better support for the developer?
Thanks in Advance