Part Number: MSP430FR5969
Tool/software: Code Composer Studio
Dear colleagues,
I have a doubt with regard to the use of the DCO and MODOSC for the ADC.
According to the MSP430FR5969 datasheet, the DCO seems more accurate and less temperature dependent (see Table 5-6 vs 5-8). In table 5-8, the current consumption of the MODOSC is specified (25 uA) but not that of DCO in Table 5-6. On the other hand, the current consumption of the ADC (table 5-22) is specified considering that the MODOSC is employed, nothing is said if the DCO is used.
I’ve been testing the ADC with DCO and MODOSC (both operating at 1 MHz) and I’ve seen that the current consumption with the DCO is significantly lower than that with the MODOSC, to be precise 128 vs 213 uA. I was wondering why the current consumption of the ADC is specified for the MODOSC if it turns out that the DCO offers more advantages in terms of accuracy, thermal stability and even current consumption.
Best regards and thanks for your time,
Ferran