Hello All,
This is Anil. i am working on the MSP430FR5994 with the I2C Communication. On a single I2C communication i have connected BQ34Z100PW-G1 and LC709203F as a slave devices. both Slaves i am using for voltage reading.
If both devices are powered(+3/+4 V for LC709203F or +12V for BQ34Z100PW-G1), then using MSP i can able to read the voltages form the IC's. But now the scenario is that, i intentionally removed the Power of BQ34Z100PW-G1, and LC709203F this is having a powered. and by MSP i am trying to read the voltage, so as per my knowledge LC709203F this one should give a voltage to MSP, but as soon as i removed the power of BQ34Z100PW-G1 then on-words MSP is not able to read the voltage from both Slaves .
In the above same situation i commented the code of BQ34Z100PW-G1, then i am getting correct results from LC709203F IC.
So , now my question is that if slave is not having Power and controller is trying to communicate with that slave plus other slaves also in I2C communication, then all slaves will fail or only NOT powered Slave device will fail?
thanks
Anil D.