This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2311: IR Reflection Sensing Reference Design

Part Number: MSP430FR2311
Other Parts Discussed in Thread: TIDM-FRAM-IRREFLECTIONSENSING

Hello TI Experts,

I ‘d like to use MSP430FR2311 to detect fire smoke~

and I have found the reference design"MSP430FR2311 Microcontroller IR Reflection Sensing Reference Design"

Do you have any testing data that can provide to me?such as accuracy?

and can it meet the standard of CCCF?

Hoping for your reply~thank you very much~

  • Hello,

    The TIDM-FRAM-IRREFLECTIONSENSING reference design is intended to demonstrate how the MSP430FR2311 MCU and its integrated analog circuits can be used for IR reflection sensing. It is not a complete fire or smoke detection product- it merely is meant to illustrate how to construct such a system using the features device, and to show the low power and ESD performance levels which are achievable. Any accuracy measurements would be specific to the hardware and IR chamber, which are not made available.

    Likewise, meeting CCCF would be the responsibility of the company/individual building and selling the end product. The reference design itself was not intended to be a reference for how to pass any CCCF requirements.

    Regards,
    Walter

**Attention** This is a public forum