Part Number: MSP430F5510
In the application note SLAA452C is written, at page 3
"MSP430 firmware upgrade over USB is implemented using the on-chip bootstrap loader (BSL) program. The BSL is located in a dedicated section of flash, outside of main program flash. TI has always provided a BSL on nearly every MSP430 device derivative, pre-programmed in the factory; but unlike other devices, the BSL on USB-equipped MSP430s uses USB as the hardware interface"
Does it mean that the I must not program anything on MSP430 flash before of the firmware upgrade ?
The microprocessor MSP430 delivers by TI contains already a BSL program in flash ?