Other Parts Discussed in Thread: MSP430F5419, MSP430F5418, TPS60213
Hi friends,
I have a new circuit board using the MSP430F5419. I cannot program it and when I turn on the power, the Vcc gets pulls way low. The uC gets slightly warm. With power off, I measure resistance from ground to Vcore, and I see 1.2 Ohms. Why is that??? Also, the resistance from Vcc to Ground is also very low, under 1 Ohm.
I have similar board using the MSP430F5418. On that one, the resistance from ground Vcore is very high, 15 MegaOhms.
I have two identical boards with the same problem. I have checked all the solder joints with a microscope. I have double checked the pinout. I have checked an identical board with no components on it, and the Vcc and Ground are not shorted on the board. It is something in the connection to the uC.
Any leads? Any specific problems with MSP430F5419?
All that I have on the circuit board is the 3.3V regulator for Vcc, the uC, a 32KHz crystal on XT1 and XT2, the reset pull-up resistor & capacitor, and a low-power voltage reference connected to Vref+. I have not programmed the uC yet. It is off-the shelf.
As I said, I have two identical boards with identical problem. I have triple-checked the pinout of all ground and Vcc connections. Vcore is connected only to a capacitor to ground. I have examined all solder joints with a microscope to check for bridging or anything wrong, and it's all picture perfect. But still I have this problem.
Please, any suggestions and help on how to diagnose this.