Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP430FR2522
Hi,
I am trying to set up the MSP430FR2433 to work on an external clock source - in XT1BYPASS Mode ( MSP-430FR2433 Launch Pad). Below is the configuration which I had used to successfully controll the MSP430FR2522 from an external clock source however this does not work on my new micro allthough I have followed the application note guidelines slau445h.
Does anyone have any suggestions of what I might be doing wrong and how to set this clock mode correctly?
Thank you,
Vlad
// Configure one FRAM waitstate as required by the device datasheet for MCLK
// operation beyond 8MHz _before_ configuring the clock system.
FRCTL0 = FRCTLPW | NWAITS_1;
P2SEL0 |= BIT0 | BIT1; // set XT1 pin as second function
CSCTL4 = SELMS__XT1CLK | SELA__REFOCLK; // Set ACLK = REFO = 32768Hz
// XT1 CLOCK = MCLK and SMCLK source
CSCTL6 = XT1BYPASS; // enable the bypass mode of operation
CSCTL5 |= DIVM_0| DIVS_1; // MCLK = XT1EXT CLOCK
// SMCLK = MCLK/2
P1DIR |= BIT0 | BIT1 | BIT2 | BIT3| BIT6; // set MCLK SMCLK and LED pin as output
P1SEL1 |= BIT1 | BIT2 | BIT3; // set MCLK and SMCLK pin as second function
PM5CTL0 &= ~LOCKLPM5;
do
{
CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault fl