This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P4111: Default BSL entry

Part Number: MSP432P4111

Hi all.

Looking at the documentation, I cannot find what is the default way to activate the UART BSL for MSP432P4111.

I'd like to know a way that works no matter the part is blank/erased or it was already flashed, without having to resort to boot override mechanism.

Datasheet states that P1.2 is BSLRXD and P1.3 is BSLTXD; but what is the pin to drive - and if it should be driven high or low - in order to entry the BSL anyway?

Furthermore, I'd like to know if such activation pin is sampled just right after reset release: if so, I could then configure an eUSCI UART over that same P1.2 and P1.3 in order to provide a wired interface to my application when BSL entry isn't forced by means of that pin.

Thank you in advance.

Best regards,

Peppe

**Attention** This is a public forum